FLIR Technical Notes

FLIR regularly publishes technical notes about FLIR infrared cameras and thermal imaging solutions.
 
 
 howfar_3d.png 

How far can you see

Often, the first question that people interested in buying a thermal imaging camera ask is “How far can I see?” This is a very reasonable question to ask, but it defies any simple answer. All FLIR Systems thermal imaging cameras are able to see the sun which is more than 146 million kilometers away from Earth. But it would be totally wrong to say that all FLIR Systems thermal imaging cameras can detect security threats at this distance.

Download Technical Note

 
 DDE_3D.png 

Digital Detail Enhancement (DDE)

The performance of an IR imaging system is often classified by its detection range. This of course makes a lot of sense for security & surveillance systems as the user will want to know how far he will still be able to “see” or detect an object such as a man or a vehicle. In practice however, it can be very hard to detect targets even though they are within the theoretical limits of the system.

Download Technical Note

 
 Fog_3d.png

Seeing through fog and rain with a thermal imaging camera

Thermal imaging cameras can produce a clear image in total darkness. They need no light at all to produce a crisp image in which the smallest of details can be seen. It makes them an excellent instrument for numerous night vision applications.

Download Technical Note

 
Wipers_3d.png

Using wipers for thermal imaging cameras.

Today, more and more people are discovering thermal imaging cameras and the benefits they have to offer. Thermal imaging cameras are being used for security and surveillance applications, to help drivers and captains navigate in the darkest of nights, help firefighters locate people in burning buildings and many other useful and sometimes even life-saving applications. Thermal imaging cameras produce a clear image in the darkest of nights, in light fog and smoke and in the most diverse weather conditions.

Download Technical Note

 
 Cooled_3d.png 

Cooled versus uncooled cameras for long range surveillance

Long-range surveillance in low-light conditions or total darkness is a perfect application for thermal imaging technology. This type of surveillance is often required at borders or for large perimeters where most threats occur at night.

Download Technical Note

 
Contact FLIR with your questions about product lines, applications or any other inquiries!