Thermal imaging cameras for flare monitoring |
||||||||||||||
Flare stacks are used in many industries to burn off unwanted waste gas byproducts, or flammable gasses released by pressure relief valves during unplanned over-pressuring of plant equipment.
Applications include oil and gas well drilling operations, oil refineries, chemical process plants, gas distribution infrastructure, and landfills. In many cases, regulations require the monitoring of a stack’s flame, or the pilot flame that ignites the gasses, to avoid having unburned hydrocarbons enter the atmosphere. |
||||||||||||||
FLIR thermal imaging cameras
Flaring is a complex processFlare systems are often a last line of defense that prevents dangerous hydrocarbon pollutants from entering the atmosphere. One example is methane, which is not only combustible, but is also 23 times more potent than CO2 as a greenhouse gas. A plant manager needs to know immediately if flare stack combustion is lost, and get the flame reignited quickly to prevent a plant shutdown. Various technologies have been tried for
monitoring the pilot flame that ignites gas flow and detects the stack
flame, with varying degrees of success. Many of these technologies are
useless or poor at minimizing smoke from stake combustion, an important
indicator of burn efficiency. One of the problems is that flare gas flows can range from low volumes during fuel gas purges in normal operations, to very large flows during emergency relief valve dumps or during total plant blowdowns. The size and brightness of the resulting stack flame, and the amount of smoke generated, depends on how much flammable material is released. Assist gases such as air or steam may be injected into the gas flow to improve combustion and help minimize smoke.
FLIR thermal imaging cameras offer a solutionFLIR thermal imaging cameras recognize the
difference in the heat signature of a flare stack flame and the
surrounding background (usually, the sky or clouds). In addition to
detecting stack flame, these cameras can be positioned to monitor the
igniter flame. Typically, cameras are mounted on a pedestal or other
rigid structure in moisture resistant housings to protect them from
harsh weather conditions.
Schematical overview of a flare detection installation The camera’s spectral response and calibration
allows it to see through moisture in the air to obtain a good image and
relative temperature reading of the flare stack or pilot flame. The
images obtained with FLIR thermal imaging cameras even allow an observer
to detect stack flame that might not be visible to the naked eye
because of its composition or low gas flow volume. This overcomes problems associated with UV flame detectors, which can be blinded by smoke. Thermal and visual images can be transmitted in real time to a central control room as either analog or digitized data. Automated ControlIn addition to visual monitoring of stack flame and smoke, automatic control of the assist gas to waste gas ratio is possible. When this ratio is properly adjusted, it improves combustion and minimizes smoke. Upset conditions require immediate adjustment of the air or steam volume to maintain proper combustion. As a bonus, automated assist gas injection control can help avoid excessive steam consumption, and provide significant cost savings.
|
||||||||||||||
Read More Application Stories |
||||||||||||||