FLIR Application Stories - Medical

FLIR regularly publishes application stories where you can read how our customers are using FLIR infrared cameras and thermal imaging solutions.
 
   

Contacte con FLIR si necesita información de línea de productos, aplicaciones, o para cualquier otra pregunta!

 
Seperator
 
The following application stories are currently only available in English
   
 
 T559325_EN.png  

Use of Infrared to detect elevated Body temperatUres

Infrared thermography can help detect elevated body temperatures which may indicate the presence of a fever. As such, the use of infrared as an adjunctive diagnostic tool to help detect people with a potential fever may contain or limit the spread of viral diseases such as bird and swine flu, or bacterial infections such as SARS.


Read Application Story            Download Application Story


 
 Erasmus 

FLIR thermal imaging cameras used to detect small nerve fiber dysfunction

It is estimated that about 2% of the world population suffers from small nerve fiber dysfunction, which can result in neuropathic pain; diabetic patients represent a large portion of this population. While the dysfunction of large nerve fibers can be assessed using standard neurological examination and electromyography (EMG), currently no noninvasive techniques exist to detect and quantify small fiber dysfunction.


Read Application Story            Download Application Story
 
 Regional block 3D.png 

FLIR thermal imaging cameras confirm effectiveness of local anesthetics

For many operations the use of local anesthetics is preferred to general anesthetics, since it is considered to be safer for the patient. But in some cases local anesthetics only work partially or not at all. To determine the effectiveness of local anesthetics the patient is subjected to pinpricks. If the patient indicates a pain sensation then the local anesthetics is considered to be ineffective.


Read Application Story            Download Application Story
 
 CEAT_3d_Small

Electronics company protects its workforce with FLIR infrared

CEAT Electronique will be ready with a defined action plan. And central to that plan is FLIR infrared. However, the FLIR camera will not be idle before or indeed after any outbreak. Thanks to its versatility it will also be used in the company's engineering laboratories.


Read Application Story            Download Application Story
 
 Charite_3d_Small

FLIR cameras help determine the functionality of anti-allergy medicine

FLIR thermal imaging cameras is one of the most efficient techniques for the study of skin temperature. It is an accurate, quantifiable, non-contact, non-invasive, diagnostic technique that allows the examiner to visualize and quantify changes in skin surface temperature using high performance thermal imaging cameras.


Read Application Story            Download Application Story


 
Erasmus_3d_Small

Infrared thermography helps to measure, chart and combat pain

To be able to chart pain, to describe it precisely and in accordance with clear criteria this is what doctors dream of and patients yearn for.

Read Application Story            Download Application Story


 
 ViralInfection_3d_Small

Keeping the spread of viral infections under control

Thermography is such a method. It has become vital to control body temperature of risk groups such as travellers and proven itself as a monitoring tool that has substantially contributed to reduce the spreading of SARS virus in many countries and regions.

Read Application Story            Download Application Story


 
Contact FLIR with your questions about product lines, applications or any other inquiries!