FLIR Orion SC7000 Series

 

The FLIR SC7000 Orion Series are infrared multispectral imagers capable of producing IR sub-band images at video rates within the SW-MWIR or LWIR region. Infrared radiation from the scene under investigation is collected through a front lens, designed to offer minimal aberration across the full IR wavelength range.

 
spectral tuning Configurable filter wheel setup to match different type of analysis
The Orion integrates a high speed 2x4 position filter wheel. It is inserted between the lens and the focal plane. The rotation of this filter wheel is driven synchronously with the     FPA clocking, such that a single image snap shot is obtained for each particular filter position.

Versatile Versatile system with traditional thermal imaging camera mode
The Orion SC7000 is capable of capturing up to 400 frames per second in 320 x 240 pixels, each high quality image being captured in snap-shot mode. The integration time is variable by software and can be different for each filter. An image is captured for each given position of the filter wheel, providing true multispectral imaging. The Orion SC7000 Series can also be used as a normal IR camera at full speed by removing or stopping the filter wheel. In addition to image acquisition, ALTAIR software also processes the acquired image data.