Vilga
Video Tracking and Image Processing Electronics
The VILGA video processor offers video tracking from multiple video sources installed in the optical payload. Targets are highlighted and overlaid on screen during tracking.
The user can select a given target amongst several proposed by the tracker. Selecting and engaging a target in tracking mode is made by the user from the hand grip controller. Once engaged the video tracker will drive the turret to the target.
The VILGA image processor |
The VILGA processor card combines multi-tasks image processing with overlaid graphics. It also offers a Picture-in-Picture mode (PIP) where two sensors can be displayed on a single display. The user can select which sensor to display as full screen in the overlaid PIP mode. The PIP mode feature is particularly useful when using the Spotter Scope (SSC) in combination with the TV zoom camera. |
Electronic stabilization |
Vilga also offers electronic stabilization of images from external sensors. This can be useful when cameras are installed on high poles or in other environments susceptible to movement caused by wind or other factors. |
Vilga tracker key features: |
• Video Tracker embedding the latest image processing algorithms |