FLIR Application Stories - Solar

FLIR regularly publishes application stories where you can read how our customers are using FLIR infrared cameras and thermal imaging solutions.
 
Solonsolar_3d_Small

Le termocamere FLIR aiutano a garantire l'impeccabile qualità dei moduli solari SOLON

Con un impianto fotovoltaico sul proprio tetto è possibile convertire la luce solare in elettricità. Ed in termini economici – gli impianti fotovoltaici sono un investimento estremamente rimunerativo. Per ottenere il massimo ritorno sugli investimenti ed un'elevata produzione nei decenni, tuttavia, l'alta qualità è un elemento chiave.

Leggi il Caso Applicativo            Scarica il Caso Applicativo
 
   

Contatta FLIR per avere maggiori informazioni sui nostri prodotti, applicazioni o per qualsiasi ulteriore richiesta!

 
Seperator
 
The following application stories are currently only available in English
 
puffpuff  

Thermal imaging inspections of roof-mounted solar panels FLIR T640 mounted on retractable pole allows to inspect hard to reach areas

As solar panels are becoming increasingly affordable, and therefore increasingly profitable, many residential homes have been fitted with solar panels in recent years. Mounting solar panels on the roof has advantages in avoiding shadows and maximizing the amount of sunlight that falls upon them, but there’s a downside as well. The high location makes it difficult to reach for thermal imaging maintenance inspections. One company came up with a creative solution to this problem: mounting the camera on a retractable mast.


Read Application Story            Download Application Story


   
 
Solar

Inspecting roof mounted solar panels with thermal imaging

The sales of solar panels are soaring, which helps to reduce CO2 emissions at electricity plants. Over time solar panels may develop defects which can be easily fixed if detected on time, but can cause a severe drop in energy production and in some cases even start a fire if left unchecked. That is why more and more solar panel installers cooperate with experienced thermographers that offer regular thermal imaging inspections to ensure the safety and effective deployment of solar systems.


Read Application Story            Download Application Story


 
Ikaros_3d_Small

Ikaros Solar uses FLIR thermal imaging cameras

More and more solar panel professionals are discovering thermal imaging as a solar panel inspection tool. One of the companies that has embraced the use of a thermal imaging camera for this purpose is the in Schoten, Belgium based Ikaros Solar.


Read Application Story            Download Application Story


 
Solartech_3d_Small

Thermal imaging cameras: fast and reliable for testing solar panels

The use of thermal imaging cameras for solar panel evaluation offers several advantages. Anomalies can clearly be seen on a crisp thermal image and - unlike most other methods - thermal cameras can be used to scan installed solar panels during normal operation. Finally, thermal cameras also allow to scan large areas within a short time frame.


Read Application Story            Download Application Story

 

 
Stiens_3d_Small

Solartechnik Stiens uses FLIR thermal imaging cameras

Many people look to the sun for a renewable power source. To make sure that the solar panels they deliver perform well, Solartechnik Stiens uses a thermal imaging camera from FLIR to look for flaws.


Read Application Story            Download Application Story

 
Contact FLIR with your questions about product lines, applications or any other inquiries!