Примеры применения FLIR - обнаружение газов

Мы регулярно публикуем материалы о том, какие новые решения с использованием тепловизионных камеры FLIR применяют наши клиенты. 
 
   

Обращайтесь в компанию FLIR, если Вас интересует ассортимент продукции, сферы применения, а также если у вас есть какие-либо другие вопросы!

 
Seperator
 
The following application stories are currently only available in English
   
T820491

Czech utility company uses FLIR GF306 optical gas imaging to check for SF6 leaks

Sulfur Hexafluoride (SF6) is used as an insulating gas in the distribution of high voltage electrical power. It allows substation equipment to be more compact. SF6 is also a very potent greenhouse gas, however. Leaks in the equipment therefore not only endanger the continuity of power distribution, the leaks also have consequences for the environment.


Read Application Story            Download Application Story
 
T820434.png    

FLIR optical gas imaging camera helps improve environment and safety at Borealis Stenungsund

Many petrochemical plants handle invisible gaseous hydrocarbons. Most of these gases pose some sort of safety aspects. They may be toxic, or can cause health issues in case of long term exposure. Others are highly flammable, explosive even, and most of them will have a negative impact on the environment if they enter the atmosphere in large quantities. That is why leak detection is of vital importance in these petrochemical plants.


Read Application Story            Download Application Story
 
T820370.png   

Environmental protection with a FLIR optical gas imaging camera

Some industrial, pharmaceutical and petrochemical plants emit gases that can harm the environment and impede the health of company employees and inhabitants of the surrounding area. Environmental protection agencies have the responsibility to make sure that these emissions fall within governmental and international policy guidelines. To help them with that task environmental protection agencies can use an optical gas imaging camera.


Read Application Story            Download Application Story
 
T559235_EN.png  

A FLIR infrared furnace camera for high temp industrial applications watches hydro reformers at German Bayernoil refinery complex

Stable high temperatures and efficient combustion in refinery furnaces, heaters and boilers are mandatory for a continuous output of high-quality oil derivates. An Infrared camera for industrial high temperature applications in hazardous areas has been developed by FLIR to keep these installations up and running efficiently.


Read Application Story            Download Application Story
 
Bayernoil_3d_Small

Bayernoil refinery uses FLIR gas detection cameras to detect leaks

Biggest refinery in southern Germany integrates a gas detection camera into its leak detection and repair programs.


Read Application Story            Download Application Story
 
BPChemicals_3d_Small

BP Chemicals enhances site safety with FLIR infrared

In the production of acetic acid BP Chemicals is world renowned and responsible for a significant proportion of world capacity. Its proprietary methanol carbonylation technology, Cativa, is in demand globally and in particular in Asia where the company continues to establish new manufacturing partnerships. In the UK its site at Saltend in East Yorkshire is not only a manufacturing flagship but also a major centre for ongoing research and development of the process.

Read Application Story            Download Application Story

 
Lindum_3d_Small

FLIR GasFindIR™ infrared camera at Norwegian landfill

Economic and environmental concerns push for an increasingly streamlined waste disposal, treatment, neutralization and recycling process. Waste treatment companies increasingly turn into energy suppliers. The GasFindIR gas detection infrared camera supports these trends by providing immediate and tangible results.

Read Application Story            Download Application Story

 
 Petroval_3d_Small

FLIR thermal imaging cameras reveal what's behind the flames

Petroval uses both cooled and uncooled thermal imaging cameras from FLIR Systems for technical audits

 

Read Application Story            Download Application Story


 
Shell_3d_Small

Tracing gas leaks: maintenance and safety problems highlighted

With more than 160,000 kilometres of piping of every imaginable kind, Shell Nederland Raffinaderij in Pernis (Rotterdam) is the largest oil refinery in Europe. Safety and environmental considerations are firmly embedded throughout the company, its quality systems and its production management processes. Shell has also adopted a stringent safety policy in which preventive maintenance is uppermost.

Read Application Story            Download Application Story


 
Vattenfall_3d_Small

Vattenfall detects hazardous gas leaks with FLIR GasFindIR LW

Vattenfall, Europe's fifth largest generator of electricity and the largest generator of heat, are among the first power companies to invest in a FLIR GasFindIR LW camera. Vattenfall use the camera for inspection of high voltage circuit breakers in interlocking installations, in order to detect leakage of the environmentally hazardous gas sulphur hexafluoride (SF6).

Read Application Story            Download Application Story


 
Contact FLIR with your questions about product lines, applications or any other inquiries!