Seeing in total darkness in a maritime environment |
|||||||||||||||||||||||
The advantages of thermal imaging.Practically all of us associate the sea with
holidays and fun, but it can be a dangerous place, especially in
nighttime and bad weather. Yachts collide with other vessels, run on
cliffs or other objects resulting in heavy damages and sometimes even
loss of life. Some of these accidents happen in open water, others while
navigating in harbors and ports.
|
|||||||||||||||||||||||
Our eyes are the first line of defense against these hazards. Unfortunately, eyes are not the best detectors at night or in bad weather. Any accident at sea does not only have severe consequences for the vessel but also for its passengers and crew. A number of tools are available to help us detect potential dangers before they become a real hazard.
Thermal imaging: an excellent tool to help you see at nightOne of these tools is thermal imaging. Thermal
imaging is the use of an infrared camera to “see” thermal energy emitted
from an object. Infrared energy can not be detected by the eye because
the energy of the photons is too low to stimulate the photoreceptors in
the eye. Also, thermal IR light does not get to the retina, because it
is highly absorbed by the eye’s lens and fluids. Infrared allows us to
see what our eyes cannot - invisible heat radiation emitted by all
objects regardless of lighting conditions. Thermal imaging cameras
produce images of invisible infrared or “heat” radiation. Based on
temperature differences between objects, thermal imaging produces a
clear image. Thermal imagers are very effective in marine
environments. They can detect objects floating in the water which may
damage a vessel, or even worse, sink it. Other vessels, shipping lane
traffic, buoys, bridges, ... it is all seamlessly detected by thermal
imaging. Although there are other technologies available for helping you to navigate during the night and to help you prevent catastrophes, thermal imaging outperforms them, has some advantages over them or it can complement them.
Bridge in total darkness(Right). Thermal image of the bridge in total darkness. Even up to several kilometers away, seeing threats is an easy task for thermal imaging cameras.
Navigation lightsThe oldest anti-collision systems on ships are
lights. In ancient times, sailors would maintain small open fires on
deck in order to be spotted by other vessels. Later these fires were
replaced by electrical navigation lights. Several types of lights serve as navigational aids
at night. But even when all boats have proper lighting, it’s very
difficult to judge bearings and closure rates. But when boats have
improper lighting, like a lot of them do, ... well, you don’t really
have a chance of avoiding an accident. Furthermore, navigation lights
become less useful when fog or rain is obstructing your view. You might
see an approaching vessel too late which can lead to lethal accidents. Thermal imaging can see through light fog and haze. Although the distance a thermal imager can see is also obstructed by light fog and haze, it will give you a clear warning of an approaching vessel, in all weather conditions.
Visualize RADAR blipsRADAR, the abbreviation of RAdio Detection And Ranging is, a system that uses reflected radio waves to determine and map the location, direction, and/or speed of both moving and fixed objects. The first commercial RADAR systems were developed during the 1940’s and today they are installed on practically every yacht.
Light amplificationLight amplification, also referred to as I2
technology, amplifies small amounts of visible light thousands of times
so that objects can be seen at night. These systems scan an area and
amplify the available ambient light to produce an image. Light
amplification does require a certain level of ambient light, but even
starlight can produce an image on a cloudless night. A high-end image
intensified camera can produce outstanding images on a clear moonlit
night. Because the system requires at least a minimum level of ambient light, conditions such as heavy overcast can limit its effectiveness. Similarly, too much light may overwhelm the system and reduce its effectiveness. Imagine yourself navigating in a harbor with the lights of the marina, or the skyline of a city, in the background. These lights will also be amplified and you will be totally blinded. Contrary to light amplification systems, thermal imaging works by detecting the heat energy being radiated. It needs no light at all and produces a clear image in the darkest environments.
Low-lux camerasThe light requirements to produce an image are
measured in lux. The lux is the rating for how well the camera sees in
low lighting conditions. The smaller the number, the less light the
camera needs to produce an image and the better the ability to see in
the dark. Low-lux cameras provide an image in an environment that is too
bright for light intensification equipment but still restricted by
darkness. But do not assume that if it is pitch black you can still see
well with a low lux camera. Contrary to a thermal imaging camera, a low lux camera will not produce an image in total darkness. Thermal imaging systems sometimes combine one or more thermal imaging cameras with a low lux camera. This gives you the ability to see during day-light and low-light conditions. Thermal imaging:more than just night time navigationThermal imagers are excellent tools for short to medium range threat detection. Today, more than ever, shipboard security is important. Thermal imaging allows you to see what is around you, even at long ranges. You can monitor activity in port or at anchor and see approaching vessels or people without alerting them that they are being watched. Each year, numerous people die after falling overboard and not being found fast enough. Finding a person that has fallen overboard within the shortest possible time-frame is of the utmost importance. Not only can the person float away from the vessel but hypothermia is an important factor to take into account. Thermal imaging can help find a person in the water before it is too late.
Thermal cameras work during the day as well, and give users the ability to see through marine haze more effectively than with the unaided eye. It is not affected by glare from the sun. Thermal imaging allows you to see through the glare, and detect possible obstacles, when navigating during sunrise or sunset. |
|||||||||||||||||||||||
Read More Application Stories |
|||||||||||||||||||||||