FLIR thermal imaging cameras help ensure continuous steel production in South Africa

Production plants have to keep running all the time. No breakdown, no downtime. To ensure proper operation of its production plants in Vanderbijlpark, ArcelorMittal South Africa uses FLIR thermal imaging cameras. This improves efficiency, safety, helps to avoid breakdowns and to minimize downtime.


The ArcelorMittal plant at Vanderbijlpark has the capacity to produce 4.4 million tonnes of liquid steel per year, which constitutes some 78% of South Africa's flat steel requirements. It is one of the world's largest inland steel mills and the biggest supplier of flat steel products in sub-Saharan Africa.

 

To keep all of the plant's equipment up and running is the task of the Condition Monitoring Team at the Reliability Engineering Department of ArcelorMittal South Africa. The team uses many condition monitoring tools, thermal imaging is one of them. "The advantage of using thermal imaging cameras is that you can see a problem developing long before it becomes visible to the naked eye, enabling you to make informed decisions regarding a suitable course of action. This leads to increased production, improved safety and increased equipment lifespan", explains Douglas Glen, Senior Thermographer at the Condition Monitoring Team.

 

Advantage of thermal imaging

Thermal imaging technology is a perfect solution, according to Glen. "You can perform thermal imaging inspections during operation and while electrical systems are under load. No downtime is required."

 

Arcelor_SA 1.png 
  Arcelor_SA 2.png 
Douglas Glen, Senior Thermographer at ArcelorMittal South Africa demonstrates the use of the FLIR P640 thermal imaging camera.   This thermal image of a high voltage capacitor shows a hot spot indicating a faulty or high resistance connection.

 

Of course thermal imaging is not the only condition monitoring tool used at the plants of ArcelorMittal South Africa. "We combine several technologies such as vibration analysis, oil analysis and inspections using thermal imaging cameras. The main advantage of thermal imaging is that you can locate mechanical and electrical problems very quickly and accurately. With thermal imaging you can immediately see which component is causing the problem."


Speed up inspections

Thermal imaging cameras also help speed up the inspections, according to Glen. "Often there are simply too many pieces of equipment for vibration analysis or other methods. We monitor 13,168 electrical panels, 6 rotating kiln furnaces, two blast furnaces, one Basic Oxygen Furnace (BOF), three large arc furnaces and several furnaces of other types. That's a lot of equipment. With our thermal imaging cameras we ensure that no fault is overlooked, while saving a lot of time."

 

According to Glen some types of equipment can only be inspected using thermal imaging cameras. "With refractory linings, for instance, thermal imaging cameras are the only practical condition monitoring tool available. With a FLIR thermal imaging camera you can scan large areas of refractory material and immediately see where the refractory insulation is failing."

 

"Before we started using FLIR thermal imaging cameras we already used cameras from Inframetrics", Glen explains. "Over a decade ago we bought our first FLIR thermal imaging camera, a PM 595, and it was immediately clear to us that FLIR was the leader in the field. Since then we have bought a P60 and recently two FLIR P640 thermal imaging cameras. All of these four FLIR thermal imaging cameras see daily use and have proved to be extremely reliable."

 

Extremely reliable

ArcelorMittal South Africa acquired their thermal imaging camera from the Johannesburg, South Africa, based FLIR products distributor Yellotec. As solution oriented company Yellotec specializes in industrial technologies. It has a long standing history with FLIR products going back almost 20 years. Yellotec can be considered to be the most experienced thermography related company in the country, because it employs the most experienced and knowledgeable personnel active in the South African Thermography market and its sales people are at least qualified to a minimum of Thermography Level 2.

 

 

Arcelor_SA 3.png   Arcelor_SA 4.png
Every week Glen and his colleagues inspect this boiler to monitor the condition of the refractory lining.
 
Arcelor_SA 5.png   Arcelor_SA 6.png
These images form part of a weekly inspection done on six Direct Reduction Iron (DRI). The images are analysed to detect refractory degradation or product build-up on the inside.

 

 

FLIR P640 thermal imaging camera

The FLIR P640 thermal imaging camera contains an uncooled microbolometer detector that produces excellent quality thermal images of 640 x 480 pixels at a thermal sensitivity of 30 mK (0.03 °C). "One of the reasons why we chose this camera – apart from the excellent image quality and accuracy – is its ergonomic design", explains Glen. "If you use a piece of equipment as often as we use the FLIR thermal imaging cameras, ergonomics and ease of use are crucial. This camera model delivers just that. Especially the tiltable viewfinder comes in handy, as it allows us to look at equipment from all possible angles."

Another reason for their choice in thermal imaging camera model was the fact that it has interchangeable optics. "This is very important for us because we also perform high voltage inspections of overhead power lines, both for our own premises and for the local municipality. For those long distance inspections a 7° angle telephoto lens is indispensible. In other situations the standard 24° lens is needed, for the telephoto lens simply has a too narrow field of view. The ability to change the lens gives the operator much more flexibility."

 

FLIR Viewer Mobile App

To facilitate comparison between new recordings and previous reports the condition monitoring personnel also has an iPod Touch attached to the left arm. "This allows us to look up previous reports so we can immediately see if anything has changed. This helps us to quickly and accurately spot defects. The added benefit of the FLIR Viewer Mobile App which we downloaded from the Apple Store is proving to be invaluable. Using the iPod Touch together with our FLIR thermal imaging cameras has enabled us to increase our efficiency by about 30%."

 

 Arcelor_SA 8.png   
Glen and his colleague Pieterse use an iPod to compare new readings with earlier inspections, using the FLIR Viewer Mobile App.
 


 

Training

The ergonomic design and ease of use of FLIR thermal imaging cameras can also be slightly deceptive, however, according to Glen. "FLIR thermal imaging cameras are so easy to use that you might think it's just a matter of point and click, but it is essential that you know what you are doing. You need extensive knowledge of thermal physics and thermal imaging technology to accurately analyze thermal images. Otherwise you will likely draw false conclusions."

 

That is why Glen and his colleagues opted for training at the Infrared Training Center (ITC), which provides training courses in cooperation with FLIR Systems. "All of our operators are ITC trained. I have a level 3 certificate, which is currently the highest level, and my colleague Nico Pieterse has the level 2 certificate."

 

With their FLIR thermal imaging cameras Glen and his team have helped ensure the continuity of production at the plants of ArcelorMittal South Africa, saving their company a lot of money in the process. Glen definitely has no regrets about choosing FLIR. "No other thermal imaging camera supplier delivers the same combination of image quality, ergonomic design and optics as FLIR", Glen concludes.

 


Read More Application Stories