FLIR användarberättelser - Forskning och utveckling |
||||
| FLIR publicerar regelbundet användarberättelser där du kan läsa om hur våra kunder använder FLIRs värmekameror för att lösa problem. |
||||
|
Thermal imaging camera helps develop new cryogenic fuel tank designFuel is a crucial part of space technology, it is necessary to propel the spacecraft but adding more fuel makes the spacecraft heavier and therefore less economic in its propulsion. Spacecraft designers continually face this dilemma. One of the best solutions current technology has to offer is the use of cryogenic fuel, due to its excellent energy to mass ratio.Read Application Story Download Application Story |
|||
|
FLIR thermal imaging camera allows evaluation of laminar designsAir flowing across an airplane’s wings will provide the lift that is essential for flight, but it also causes friction and drag, which slows down the aircraft and causes inefficient propulsion. Laminar air flow along an airplane’s wings can theoretically greatly reduce drag, improving the airplane’s efficiency.Read Application Story Download Application Story |
|||
![]() |
Adidas, improving the comfort of athletes worldwideSatisfying professional athletes is not an easy job. They demand the best quality equipment available on the market in order to perform at their best. But also the recreational sportsmen and woman insist on having excellent material. A FLIR Systems infrared camera,the ThermaCAM™ SC 3000, helps them to achieve this goal. Read Application Story Download Application Story |
|||
![]() |
Ancona uses FLIR Systems ThermaCAM™ SC 3000 for research.Universities are using infrared thermography to do both fundamental and applied research. A perfect example is the research that professor Ricci and Prof. Cesini are conducting at the university of Ancona in Italy.Read Application Story Download Application Story |
|||
![]() |
FLIR Systems infrared camera at the university of AnconaInfrared thermography is a non-contact and non-invasive temperature measurement technique. It requires a very short experimental set-up and gives excellent results. These are some of the reasons why the University of Ancona is using a FLIR Systems ThermaCAM™ in its research programs.Read Application Story Download Application Story |
|||
|
FLIR Advanced Thermal Solutions
Thermal cameras are today being used in many different ways as more and more people realize the potential of this powerful imaging technology. Thermal cameras made by FLIR play pivotal roles in a wide range of industrial, commercial and government activities in more than 60 countries worldwide. Read Application Story Download Application Story |
|||
![]() |
ThermaCAM™ shows hidden billiards physicsMozart, Einstein, kings and emperors, nobles and commons adored it. The earliest mentioning of billiards dates from the 15th century. Since then, the game has developed into local variations: billard, snooker, pool, carambol, pyramid, to mention just a few.Read Application Story Download Application Story |
|||
![]() |
FLIR thermal imaging cameras help detect material failures in bikesModern bike frames are made of carbon fiber-reinforced plastics, which is exceptionally light and strong. But the way these frames behave in case of failure is fundamentally different from the old metal frames. Instead of bending, carbon fiber-reinforced plastics break. This exposes riders to dangerous situations; failures can lead to injury or even death.
|
|||
![]() |
Thermography shows why champagne should be poured differentlyThe university’s most recent discovery is that the way champagne is currently poured, causes loss of aroma and thus of taste. The researchers claim that champagne should be served like beer. Thermographic cameras have played a vital part in this recent discovery. |
|||
![]() |
John Deere, use FLIR Systems ThermaCAM™ infrared camera to optimize its tractorsTractors are one of the most known manufacturing core businesses of John Deere. Their reliability depend on the quality and versatility of the latter’s engines, which have to perform in harsh, dusty and muddy working environments and deal with vast temperature differences. They have to pass severe acceptance tests.Read Application Story Download Application Story |
|||
![]() |
FLIR Systems assists NASA in improving safety in spaceThe NASA Langley Research Center has chosen the FLIR Systems ThermaCAM™ S65 as the preferred infrared camera system for its current shuttle and International Space Station programs.Read Application Story Download Application Story |
|||
![]() |
FLIR SC7600 used for biomass power plants inspection and optimizationThw research at Risø DTU is performed within several research divisions (biosystems, fuel cells, materials, radiation, systems analysis, wind energy, plasma physics and solar energy). Among the on-going research themes, biomass combustion is making large use of infrared imaging technology for about eleven years |
|||
![]() |
The Art of FLIR SuperframingWhat is a good thermal image? It is an image which presents a high contrast, while showing the smallest temperature differences. Thermal imaging cameras are able to do that, but within a defined temperature range. Read Application Story Download Application Story
|
|||
![]() |
FLIR Systems cameras used to monitor active volcanoesIf an infrared camera is the instrument to detect and measure hot spots, it must be the perfect tool to survey the biggest and most impressive hot spots on earth: volcanoes. |
|||
| Contact FLIR with your questions about product lines, applications or any other inquiries! |
||||