1. What methods are available to acquire digital data using Photon?
2. What is needed in order to create my own application to control and/or acquire digital data using Photon?
3. Is Photon’s 14-bit digital output (serial LVDS) true usable 14-bit data from the array?
4. Is the digital data from Photon signed or unsigned integer?
5. Is there Linux support for Photon?
6. Can the camera be completely controlled using a PCI-1422 frame grabber card?
7. Can the camera accept an external sync from the PCI-1422 to command the camera to digitize imagery at 30 frames per second?
8. Is there another way for the camera to accept an external sync using the PCI-1422?
9. Can the frame grabber be used to command the camera to perform a NUC ‘on demand’?
10. Can the frame grabber be used to turn on and off AGC and adjust contrast and brightness? Can we read out the NUC parameters from the camera?
11. Can the camera data be streamed to disk over the PCI-1422 card and displayed real time?
12. Does the digital zoom feature affect the LVDS output?