1. What is needed in order to create my own application to control and/or acquire digital data using Photon?
2. What are the lens options and the minimum focus lengths for the Photon? What is the range of focus? Is it possible to adjust the focus of Photon lenses manually?
3. Can two cameras be set up as master and slave for synchronization purposes?
4. Is there Linux support for Photon?
5. What is the function of the 30-pin connector and the optional 15-pin connector on the Photon? What is the function of the 30-pin connector and the optional 26-pin connector on the Photon 640?
6. Is there a recommended connector or cable harness that can be used to interface to the SAMTEC 30-pin connector?
7. What is the voltage on the serial port? Do I need to access the serial port for normal operation? I am trying to connect to the camera via HyperTerminal and I can’t seem to get any control or response. I’ve tried a Null modem cable and a straight-thru cable and can’t seem to connect.
8. What is needed to use Photon cameras?
What type of connector is used for the power? What is the polarity of this connector?
9. Can I just hook a Photon up to power and a monitor?
10. What is the I/O module and how does it differ from going directly into a monitor or PC?
11. What methods are available to acquire digital data using Photon?
12. The Photon 30-pin interface control drawing shows the pin numbers reversed for the interface connector J1 (SAMTEC TFML-115-02-S-D-P), in comparison with SAMTEC’s drawing for TFML-115-02-S-D-P. Which reference is correct?
13. What would be needed to integrate Photon on a vehicle and run it?
14. For Photons used on vehicles for driver vision enhancement or situational awareness, how would the operator inside view the scene?
15. Is Photon’s 14-bit digital output (serial LVDS) true usable 14-bit data from the array?
16. Can the camera be completely controlled using a PCI-1422 frame grabber card?
17. Can the camera accept an external sync from the PCI-1422 to command the camera to digitize imagery at 30 frames per second?
18. Is there another way for the camera to accept an external sync using the PCI-1422?
19. Can the frame grabber be used to command the camera to perform a NUC ‘on demand’?
20. Can the frame grabber be used to turn on and off AGC and adjust contrast and brightness? Can we read out the NUC parameters from the camera?
21. Can the camera data be streamed to disk over the PCI-1422 card and displayed real time?
22. Is it possible to use the Accessory Kit for the Photon 320 (P/N 421-0021-00) with a Photon 640 camera?
23. What is the input power range for the Ethernet module?