1. How can I figure out which lens version will work best for my application?
2. Is it possible to get the Photon camera with an athermal lens?
3. I need to use the Photon to image an object at close range. Is it possible to adjust the focus of Photon lenses manually? What is the range of focus? What is the close focus distance?
4. If a lens-less camera core is purchased, how can it be calibrated with a lens?
5. What are the lens options and the minimum focus lengths for the Photon? What is the range of focus? Is it possible to adjust the focus of Photon lenses manually?
6. Is the spectral response of the microbolometer array 7.5µ to 13.5µ, or is the spectral response a function of the lens?
7. Should I clean the Photon lens, and how?
8. How do water droplets on the camera lens affect the image? Do they affect the image as much as a on a visible light range camera?
9. Is there a good reflector for IR? Can a standard front surface mirror be used or are there other materials available?
10. What are the detection ranges for the various Photon/lens versions?
11. Can the Photon camera be pointed at the sun?
12. Does the digital zoom feature affect the LVDS output?
13. What material is used for the Photon 320 sensor window? Does the window have an anti-reflection (A/R) coating? Can I use a Photon 320 to image below 8µ?