| |
Question:
How far can I see with the PathFindIR?
Answer:
This depends upon how large the object is and what the difference in temperature of the object to the ambient temperature at that time. The road and upcoming turns will be visible for thousands of feet, pedestrians, and animals such as deer usually can be detected 4 times further than with standard headlights. Since the PathFindIR has a 36 degree field of view, it will display not only the road ahead, but, also both sides of the road and well into the ditches where animals tend to graze. Your headlights only show you what is in front at distances about 450 feet. PathFindIR will significantly increase your viewing distance and give you the added wider field of view and therefore increase your reaction time.
|