FLIR News & Events

 
Home
Investors
FLIR Jobs
Tradeshows




 
 

FLIR News
Discover the FLIR Scout Handheld Thermal Camera

You saw it at CES and have been waiting to get your hands on the FLIR Scout thermal camera.  The wait is over!  

FLIR Scout

This is a great camera for everyone.  Whether you're hiking, fishing, camping or just trying to entertain the kids in the backyard, the FLIR Scout is the thermal camera for you.  Want to try it before you buy it?  Check out the interactive simulator.   



FLIR at SPIE

If you're in Orlando this week for SPIE (Defense, Security and Sensing show) stop by the FLIR booth, #703.  We're here with our latest core, the Tau 640, as well as many of our other cores and thermal cameras.



FLIR Introduces Tau 640 Thermal Core

Last week at ISC West, FLIR launched the Tau 640 thermal core.  This is the smallest and most powerful core available. If you pull apart any of our latest high resolution cameras the Tau 640 is what you will find.  It is a 640x480 LWIR uncooled focal plane array (FPA) camera with a pixel size of 17 microns.  A great addition to the core family.



FLIR at Palm Beach International Boat Show

Spring is here and it's a perfect time to think about your boat.  If you're in West Palm Beach, the best place to think about your boat is at the Palm Beach International Boat Show.   We'll be located in #588 and #589 since we have so much to show you, like the M-Series thermal cameras and the handheld First Mate.  See you there!



Sport Fishing and the M-Series single payload

Sport Fishing Magazine features an article on the new FLIR M-Series single payload.  It's the perfect camera for the sport fisherman's boat or any other vessel that needs a thermal camera without the additional cost of an added low light camera.  



FLIR receives Innovation Award in Miami

At the recent Miami Boat Show, the FLIR First Mate was recognized at the Innovation Awards as a great addition to your vessels safety equipment.  It's a little hand held thermal camera that packs a lot of night vision power.  It's perfect for man over board emergencies as well as night time navigation. 



FLIR at Miami Boat Show

Next week FLIR will be at the Miami Boat Show to show off the latest FLIR First Mate handheld thermal camera and the FLIR M-Series thermal camera.  We'll be in booth #1657.  Also, look out for our street team wandering around the show demonstrating the FLIR First Mate.



FLIR First Mate receives 2010 Pittman Innovation Award from Sail Magazine

The FLIR First Mate has been awarded a 2010 Pittman Innovation Award from Sail Magazine in the safety gear category.  The FLIR First Mate thermal hand held maritime camera is ideal for MOB emergencies and navigating at night. 

FLIR First Mate



FLIR Introduces Full line of Affordable IP Thermal Cameras

Portland, OR – January 22, 2010 – FLIR Systems, Inc. (NASDAQ:FLIR), the world’s leading manufacturer of thermal security cameras, announced the release of a full range of affordable IP thermal security cameras with models available for as little as $3,495.

This new spectrum of thermal cameras provides low-cost additions to FLIR’s groundbreaking F- and PT-Series of IP thermal security cameras. They feature 160 × 120 pixel resolution and have three available lenses, ranging from the wide-angle 24° lens to the narrow 12° lens for maximum imaging and integration flexibility.

Available as either a fixed-site (thermal only) configuration, or as pan/tilt multi-sensor systems with an integrated daylight camera, this array of affordable IP thermal cameras complements FLIR’s existing line of higher resolution F- and PT-Series cameras, extending their industry leading product lineup with a range of lower cost, lower resolution thermal security cameras.

Even though they are affordable, these high performance thermal cameras still provide easy integration over open IP network standards, and dual channels of streaming digital video in H.264, MPEG-4, or MJPEG formats, allowing users to mix and match formats to meet various viewing and recording requirements

With their innovative imaging cartridge design, all F- and PT-Series thermal security cameras can be quickly and easily upgraded in the field to 320 × 240 or 640 × 480 resolution cameras.

All F- and PT-Series thermal security cameras come with FLIR Sensor Manager, a complete sensor networking software package that provides full network control and video display, and advanced features like geo-referenced threat mapping, pan/tilt slew-to-cue, and powerful video analytics creating a complete perimeter security solution.



West Marine University 2010

Look for us next week at West Marine University 2010 in Monterey.  We'll be in booth #407 with the FLIR First Mate handheld thermal camera, the FLIR M-Series and a Navigator II on display.  Looking forward to seeing you there!



FLIR Night Vision in Audi and Rolls Royce

Motodash has an article published about FLIR technology in a few big name cars.  Both the 2011 Audi A8 and 2010 Rolls Royce Ghost Night Vision system feature the same see at night technology you will find in the FLIR PathFindIR.  FLIR has already been featured in the BMW 5, 6 and 7 series.  Check out the video that demonstrates how much more you can see at night with a FLIR PathFindIR than with regular headlights.



FLIR at the Shot Show and the New York Boat Show

We're hitting two trade shows this week!  If you are in Las Vegas this week for the Shot Show, come visit us at the Sands! Our booth will be in US Night Vision (#12873).  If you have been wanting a chance to check out the thermal night vision handheld FLIR H-Series, this is your chance.  

We'll also be at the NY Boat Show this week showing off the mounted thermal night vision FLIR M-Series and the thermal night vision handheld FLIR First Mate.  

Come check us out and our amazing ability to be at two places at once and see at night at the same time.



FLIR Scout introduced at CES

For those of you who missed us at CES, let me introduce you to FLIR Scout.  The green first cousin of the FLIR H-Series, the FLIR Scout is perfect for the outdoor enthusiast.  Check out this video from CES that shows the camera in action.  The camera was also featured at show stoppers. Look for more about the FLIR Scout in the coming months.



FLIR at CES 2010

FLIR will be at CES in Las Vegas next week.  We'll be in booth #531 showing off a plethora of security cameras, including a FLIR H-Series.  Also making an appearance will be the FLIR First Mate, FLIR M-Series and FLIR PathFindIR.  Looking forward to seeing everyone there!



Police Magazine calls FLIR H-Series a IACP 2009 Best in Show

If you happened to make it to the International Association of Chiefs of Police (IACP) this year we hope you stop by the FLIR booth and checked out the FLIR H-Series.  Police Magazine did and they are calling the FLIR H-Series handheld thermal camera a best in show!

FLIR H-Series



 


  © 2011 FLIR Systems. All rights reserved. Images/content for illustration purposes only. Privacy Policy. Copyright Policy. Terms of Use.