Everything around you either emits or reflects heat energy. Thermal imaging makes the otherwise invisible world of heat energy visible to your eyes. Visible light doesn’t affect the thermal world, so you can see equally well in highly lit and totally dark environments — the thermal image is the same. This allows you to visualize the effects of many real-world events and conditions that are otherwise impossible to detect. There are countless new, useful, and fun ways thermal imaging will integrate into your daily life. The list of uses is long and will grow dramatically when the consumer world begins to See the Heat.


HOW IT WORKS:

FLIR ONE™ is a non-contact device that detects infrared energy (heat) and converts it into an electronic signal, which is then processed to produce a thermal image on your phone screen and perform temperature calculations. Heat sensed by an infrared camera can be very precisely measured, allowing you to use the FLIR ONE™ in a variety of practical and fun ways by revealing a thermal world not visible to the unaided eye.

LEARN MORE


GALLERY

Thermal images shown are for illustration purposes only, and may not have been taken by the camera series depicted.