The following apps are not yet compatible with the next generation of FLIR ONE (Gen 3). These apps only operate on the Gen 2 iOS and Android devices.
A full list of apps compatible with the next generation models will be available soon.
In addition to the official FLIR apps, we've built a showcase of the best of breed apps written for the FLIR ONE. When your app achieves FLIR Approved App status, it will automatically be added to the gallery.
App for conducting simple and accurate insulation audits on your home by utilization of the FLIR ONE. The app can detect any anomalies in the heat signatures through the walls of your home and begin to diagnose any possible problems with the current insulation. From here, the app can recommend products and solutions to correct the flaw.
Available Now !
The Apps listed on this page have been reviewed and approved by FLIR and have been given the “FLIR Approved” status, which is verification that the App conforms to FLIR’s corporate guidelines and policies for appropriate content and user experience. FLIR does not review the App for compliance with Intellectual Property rights, safety, or other potential factors that may result in liability to the Developer; thus FLIR disclaims any and all liability that may arise through a third party’s use of the App or whether the App will meet any quality standard or level of merchantability.
What does FLIR Approved app mean and what's the process for getting an app approved?
FLIR Certified Developers are trained by FLIR on thermal imaging and FLIR ONE developer tools. Want to become one of the elite certified developers?
Word Word
AquaCheck uses the FLIR One camera to analyze the surface temperature of a body of water and based on a relative comparison to your own skin's temperature, informs you of how comfortable it would be to do some swimming!
Boat Beacon uses AIS to show the positions of ships around you when at sea including bearing and distance and closest point of approach (CPA). It also has a Marker button (MOB) which you can use to mark a spot and track its location. Boat Beacon's Augmented Reality view shows the ship positions, a thermal view, and MOB overlaid on the live Camera View.
A mobile application for conducting simple and accurate insulation audits on your home by utilization of the FLIR One Thermal Camera. The app can detect any anomalies in the heat signatures through the walls of your home and begin to diagnose any possible problems with the current insulation. From here, the app can recommend products and solutions to correct the flaw.
FLIR ONE Paint is an easy way to capture color photos and convert selected elements from color to thermal with the swipe of your finger. So you can create images that make selected objects really stand out!
FLIR ONE ThermometerFLIR ONE Thermometer turns your FLIR ONE Thermal Camera into a thermometer. Align the cross hair into the zone you want to measure and the temperature will be displayed in the LCD screen.
Electrical testing and inspection previously only possible on expensive desktop software, is now available on your iPhone/iPad.
iCertifi not only produces high quality BS 7671 electrical certificates, it's also an assistant monitoring and checking your test results and calculating data where appropriate, which makes testing more accurate and productive.
With the FLIR One camera, Meat Monitor can gauge the quality of meat storage by pointing your phone at your meat of choice. This is ideal for situations in the supermarket or grocery store in which you are unsure of the condition of the meat. The app will provide a grade and suggestion based off of USDA guidelines for meat storage.
NovaVision for FLIR ONENovaVision utilizes the thermal image processing from the FLIR One to create thermal goggles for the user. The screen is divided in half and each half contains an image view, where the content comes directly from the FLIR One.
"FLIR ONE Burst Mode" lets you take and save multiple versions of a single image using different thermal color palettes, all with the click of a button.
Thermal CompareThermal Compare is a revolutionary companion app for the FLIR One! It makes your FLIR One thermal sensor Contextually Aware, it automatically groups your Thermal Images using your GPS, it gives you help lining up your photos with Smart Guide overlays, it makes Thermal Surveys easy with a simple User Experience, and it remotely views the Thermal Image Camera feed on your Apple Watch!
Thermal PresoThis mobile application is designed to better display the image from the FLIR One thermal camera to a widescreen monitor or television. The sidebars allow for the new resolution while dynamically blending the image for a pleasing appearance. Primarily used in public showings and displays of the FLIR Technology.
Thermal Scavenger HuntCreate and manage fun and educational scavenger hunts using thermal imaging to let players view their environment in a whole new way.
Innovative "green screen" app uses thermal imaging to isolate and extract a subject's body and then project it into a different background.
Thermal SentryA mobile application which utilizes the FLIR ONE in order to create the functionality of a thermal motion detection sentry. The application can detect the movement of temperature anomalies and generate an alarm if the selected accepted degree of motion is exceeded. Due to the high contrast in the thermal signature of a living being and the static background, this method of motion detection is impressively accurate.
Thermix is the first multimodal social network for thermal videos. You can easily take and share your videos openly with the world or privately with your selected friends. In addition, Thermix provides a free cloud storage service for your footages. Join us in the discovery of the thermal world, now in a more connected way.
Vernier Thermal AnalysisScience education app teaches & entertains with thermal imaging.
Zombie Vision turns your FlIR ONE Thermal Camera accessory into a realtime zombify viewer. Everyone you see through the camera will look like zombies.
EverfaveHome DIY energy efficiency app that uses GPS and publicly available home info to walk a user through the process of inspecting their home for potential energy efficiencies or heat-related problems and then recommends nearby contractors to address them.
FieldLens Thermal FLIR ONEProfessional construction job management tool that uses thermal imaging to identify various jobsite problems and team collaboration tools to manage repair processes. Waiting to release with Android version.
Grafheati is an iOS app for FLIR ONE that lets you virtually “tag” anything using a hair dryer instead of a spray can! Choose a background canvas or take one with your iPhone camera, grab your hair dryer and “spray” grafiti on it. Then use in-app editing tools to make it perfect and upload the saved image using in-app sharing tools. Tag stuff, entertain your friends, and don’t go to jail for it!
Manything FLIR ONE turns your iOS device into a thermal night vision monitoring camera in seconds. Features include live streaming, cloud recording, motion detection, remote control and temperature alerts.
Mu-Therm is a low-cost portable and fast non-contact mass human temperature screening system for determining hyperthermic persons. Mu-Therm automatically identifies and determine temperatures of all faces in the thermal image, and simultaneously displays the associated temperature values in the typical color image. Highlighted temperature in red and sound warning are activated when there is at least one hyperthermic person in the image.
PhoenixMobile for AppraisersPhoenixMobile - the leading data gathering app for Real Estate Appraisers. It's time to throw your clipboard in the trash.
BulldozAIR - Construction work made easy for your team: contractor, architect, factory. Manage your punchlist, plans, blueprints, RFI, construction project, building sites. Winner of the Innovation Trophy at BATIMAT World Construction Expo BulldozAIR is a free construction app for your team. It enables owners, contractors, architects, project managers, superintendents, manage their construction projects. BulldozAIR keeps all the plans, blueprints and project documentation in one place. An issue is spotted on a note with pictures, drawings, sketches, measures, localisation. BulldozAIR is used in RFIs, punchlist, checklist, markups, sites supervision, maintenance, building construction, infrastructure, audit, quality control, security controls, and works for all companies during all the project duration and not only at the end.
ThermOL2RIndustrial preventative maintenance app. ThermOL2R calculates the compensation values for machine thermal growth when performing shaft alignment, using real-time thermal images temperatures measured whit the FLIR ONE® camera.
ThermoPro is an app for managing thermal images from the FLIR ONE™ camera. The app features a full hierarchical database for tracking points of interest over time. Create instant reports that include the thermal image, GPS location, non-thermal picture of asset, notes, and signature. Thermal images can be drawn over and annotated in reports to point out problem hot spots. Tap anywhere on captured images to determine temperature at a given spot. Full integration with ThermoPro web app provides reporting and analysis from any computer. Web app reports include full area reports, asset reports, and individual measurement reports. Direct upload from the iPad app makes getting data into the web app fast and easy. Uses of the app include home inspection, pest infestation, power line maintenance, construction, electrical system testing, mechanical equipment health assessment and tracking fluid system tank levels/line blockages/pipe temperatures. ThermoPro is the complete solution for professionals managing thermal images from the FLIR ONE™ camera.
This application monitors your baby during sleep and raises alarm if he/she is out of rectangular Region of Interest defined by you.
A Professional Bearing Compass designed to help navigate at sea and used much like a pair of Compass Binoculars. When held vertically it shows the real-time camera view with a compass, bearings and artificial horizon overlaid, when flat it shows a real time map centred on where you are with the bearings and compass overlaid.
NovaVisionNovaVision utilizes the thermal image processing from the FLIR One to create thermal goggles for the user. The screen is divided in half and each half contains an image view, where the content comes directly from the FLIR One.
Remote Thermal Cam f. FLIR ONERemote Thermal Cam is a useful Android app that lets you use Your FLIR ONE as a Webcam for Your PC by sending an MJPEG stream to a SmartCam server via WiFi.
Thermal Camera for FLIR ONEThermal Camera uses the Flir One v2 to display a live infrared image. To achieve this task it uses its own render mechanism, that uses the 14bit raw data from the Flir SDK. Due to the nature of this implementation it can add new features, which are Flir independent.
Thermori-onThermori-on is a thermal musical instrument, inspired by the "Tenori-on", and using your FLIR thermal imaging camera.
ThermoVisual Motion Detector (TVMD) is an intelligent, easy to use application that detects thermal and/or visual motion or changes automatically by using FLIR ONE infrared camera.
With Thermal Paint you can draw areas of the thermal image on top of the aligned visible-light image from the FLIR One. Highlight important areas of an image, or get creative and create unique works of art.
Word Word
AquaCheck uses the FLIR One camera to analyze the surface temperature of a body of water and based on a relative comparison to your own skin's temperature, informs you of how comfortable it would be to do some swimming!
Boat Beacon uses AIS to show the positions of ships around you when at sea including bearing and distance and closest point of approach (CPA). It also has a Marker button (MOB) which you can use to mark a spot and track its location. Boat Beacon's Augmented Reality view shows the ship positions, a thermal view, and MOB overlaid on the live Camera View.
A mobile application for conducting simple and accurate insulation audits on your home by utilization of the FLIR One Thermal Camera. The app can detect any anomalies in the heat signatures through the walls of your home and begin to diagnose any possible problems with the current insulation. From here, the app can recommend products and solutions to correct the flaw.
FLIR ONE Paint is an easy way to capture color photos and convert selected elements from color to thermal with the swipe of your finger. So you can create images that make selected objects really stand out!
FLIR ONE ThermometerFLIR ONE Thermometer turns your FLIR ONE Thermal Camera into a thermometer. Align the cross hair into the zone you want to measure and the temperature will be displayed in the LCD screen.
Electrical testing and inspection previously only possible on expensive desktop software, is now available on your iPhone/iPad.
iCertifi not only produces high quality BS 7671 electrical certificates, it's also an assistant monitoring and checking your test results and calculating data where appropriate, which makes testing more accurate and productive.
With the FLIR One camera, Meat Monitor can gauge the quality of meat storage by pointing your phone at your meat of choice. This is ideal for situations in the supermarket or grocery store in which you are unsure of the condition of the meat. The app will provide a grade and suggestion based off of USDA guidelines for meat storage.
NovaVision for FLIR ONENovaVision utilizes the thermal image processing from the FLIR One to create thermal goggles for the user. The screen is divided in half and each half contains an image view, where the content comes directly from the FLIR One.
"FLIR ONE Burst Mode" lets you take and save multiple versions of a single image using different thermal color palettes, all with the click of a button.
Thermal CompareThermal Compare is a revolutionary companion app for the FLIR One! It makes your FLIR One thermal sensor Contextually Aware, it automatically groups your Thermal Images using your GPS, it gives you help lining up your photos with Smart Guide overlays, it makes Thermal Surveys easy with a simple User Experience, and it remotely views the Thermal Image Camera feed on your Apple Watch!
Thermal PresoThis mobile application is designed to better display the image from the FLIR One thermal camera to a widescreen monitor or television. The sidebars allow for the new resolution while dynamically blending the image for a pleasing appearance. Primarily used in public showings and displays of the FLIR Technology.
Thermal Scavenger HuntCreate and manage fun and educational scavenger hunts using thermal imaging to let players view their environment in a whole new way.
Innovative "green screen" app uses thermal imaging to isolate and extract a subject's body and then project it into a different background.
Thermal SentryA mobile application which utilizes the FLIR ONE in order to create the functionality of a thermal motion detection sentry. The application can detect the movement of temperature anomalies and generate an alarm if the selected accepted degree of motion is exceeded. Due to the high contrast in the thermal signature of a living being and the static background, this method of motion detection is impressively accurate.
Thermix is the first multimodal social network for thermal videos. You can easily take and share your videos openly with the world or privately with your selected friends. In addition, Thermix provides a free cloud storage service for your footages. Join us in the discovery of the thermal world, now in a more connected way.
Vernier Thermal AnalysisScience education app teaches & entertains with thermal imaging.
Zombie Vision turns your FlIR ONE Thermal Camera accessory into a realtime zombify viewer. Everyone you see through the camera will look like zombies.
EverfaveHome DIY energy efficiency app that uses GPS and publicly available home info to walk a user through the process of inspecting their home for potential energy efficiencies or heat-related problems and then recommends nearby contractors to address them.
FieldLens Thermal FLIR ONEProfessional construction job management tool that uses thermal imaging to identify various jobsite problems and team collaboration tools to manage repair processes. Waiting to release with Android version.
Grafheati is an iOS app for FLIR ONE that lets you virtually “tag” anything using a hair dryer instead of a spray can! Choose a background canvas or take one with your iPhone camera, grab your hair dryer and “spray” grafiti on it. Then use in-app editing tools to make it perfect and upload the saved image using in-app sharing tools. Tag stuff, entertain your friends, and don’t go to jail for it!
Manything FLIR ONE turns your iOS device into a thermal night vision monitoring camera in seconds. Features include live streaming, cloud recording, motion detection, remote control and temperature alerts.
Mu-Therm is a low-cost portable and fast non-contact mass human temperature screening system for determining hyperthermic persons. Mu-Therm automatically identifies and determine temperatures of all faces in the thermal image, and simultaneously displays the associated temperature values in the typical color image. Highlighted temperature in red and sound warning are activated when there is at least one hyperthermic person in the image.
PhoenixMobile for AppraisersPhoenixMobile - the leading data gathering app for Real Estate Appraisers. It's time to throw your clipboard in the trash.
BulldozAIR - Construction work made easy for your team: contractor, architect, factory. Manage your punchlist, plans, blueprints, RFI, construction project, building sites. Winner of the Innovation Trophy at BATIMAT World Construction Expo BulldozAIR is a free construction app for your team. It enables owners, contractors, architects, project managers, superintendents, manage their construction projects. BulldozAIR keeps all the plans, blueprints and project documentation in one place. An issue is spotted on a note with pictures, drawings, sketches, measures, localisation. BulldozAIR is used in RFIs, punchlist, checklist, markups, sites supervision, maintenance, building construction, infrastructure, audit, quality control, security controls, and works for all companies during all the project duration and not only at the end.
ThermOL2RIndustrial preventative maintenance app. ThermOL2R calculates the compensation values for machine thermal growth when performing shaft alignment, using real-time thermal images temperatures measured whit the FLIR ONE® camera.
ThermoPro is an app for managing thermal images from the FLIR ONE™ camera. The app features a full hierarchical database for tracking points of interest over time. Create instant reports that include the thermal image, GPS location, non-thermal picture of asset, notes, and signature. Thermal images can be drawn over and annotated in reports to point out problem hot spots. Tap anywhere on captured images to determine temperature at a given spot. Full integration with ThermoPro web app provides reporting and analysis from any computer. Web app reports include full area reports, asset reports, and individual measurement reports. Direct upload from the iPad app makes getting data into the web app fast and easy. Uses of the app include home inspection, pest infestation, power line maintenance, construction, electrical system testing, mechanical equipment health assessment and tracking fluid system tank levels/line blockages/pipe temperatures. ThermoPro is the complete solution for professionals managing thermal images from the FLIR ONE™ camera.
This application monitors your baby during sleep and raises alarm if he/she is out of rectangular Region of Interest defined by you.
A Professional Bearing Compass designed to help navigate at sea and used much like a pair of Compass Binoculars. When held vertically it shows the real-time camera view with a compass, bearings and artificial horizon overlaid, when flat it shows a real time map centred on where you are with the bearings and compass overlaid.
NovaVisionNovaVision utilizes the thermal image processing from the FLIR One to create thermal goggles for the user. The screen is divided in half and each half contains an image view, where the content comes directly from the FLIR One.
Remote Thermal Cam f. FLIR ONERemote Thermal Cam is a useful Android app that lets you use Your FLIR ONE as a Webcam for Your PC by sending an MJPEG stream to a SmartCam server via WiFi.
Thermal Camera for FLIR ONEThermal Camera uses the Flir One v2 to display a live infrared image. To achieve this task it uses its own render mechanism, that uses the 14bit raw data from the Flir SDK. Due to the nature of this implementation it can add new features, which are Flir independent.
Thermori-onThermori-on is a thermal musical instrument, inspired by the "Tenori-on", and using your FLIR thermal imaging camera.
ThermoVisual Motion Detector (TVMD) is an intelligent, easy to use application that detects thermal and/or visual motion or changes automatically by using FLIR ONE infrared camera.
With Thermal Paint you can draw areas of the thermal image on top of the aligned visible-light image from the FLIR One. Highlight important areas of an image, or get creative and create unique works of art.
2017 © FLIR® Systems, Inc. All rights reserved.
Privacy Policy | Copyright Policy | Terms of Use