|
 |
 |
|
|
An infrared camera can be installed on ships. Infrared cameras can not only be installed on yachts but also commercial vessels can benefit from the power of an infrared camera. Thanks to an infrared camera, captains can navigate safely at night. Infrared can detect buoys, outcroppings of land, small vessels, … An infrared camera can even detect small objects that go undetected by radar but can harm a vessel severely. An infrared cameras can complement radar.
|
| |
|
|
|
|
Security professionals are using the power of infrared cameras to see in the darkest of nights.
An infrared camera can compliment and complete a security camera network. Infrared cameras are providing the power to see threats invisible to the naked eye, turning night into day. An infrared camera makes images from the heat energy that is around us all the time, not from reflected visible light, giving you true 24/7 imaging capability without lights or illuminators.
|
|
|
|
|
|
|
|
Infrared cameras are widely used for Homeland Security. Thanks to the ability of an infrared camera to detect human-sized targets several kilometers away, an infrared camera is extremely suited for border surveillance and protection. Some FLIR Systems infrared cameras can detect human-sized targets at a distance of practically 20 kilometers away.
|
| |
|
|
|
|
Infrared cameras are widely used by law enforcement officers worldwide. An infrared camera gives them the ability to see without being seen. For this application FLIR Systems not only markets fixed mounted infrared cameras but handheld infrared cameras as well.
Infrared cameras can help border control professionals to meet the demands they face at night and in other low-light situations. Infrared cameras can be integrated in a border security project with radars and other sensors in a so called “slew-to-cue” mode. |
| |
|
|
|
|
An infrared camera can be incorporated in cars, busses, trucks, trains, … for driver vision enhancement. An infrared camera sees up to 5 times further than headlights. Thanks to infrared cameras the driver can see pedestrians and obstacles on the road from a further distance. This way an infrared camera can help to avoid deadly accidents.
|
| |
|
|
|
|
FLIR Systems also markets infrared cameras that have been especially developed for aviation applications. Mounted on an aircraft, an infrared camera can be used for pilot vision enhancement.
|
| |
|
|
|
|
Infrared cameras have become increasingly popular the last years, Thanks to an increase in volume, the price of infrared cameras has come down. Today, more and more manufacturers are interested in integrating a infrared camera in their own product. For OEM manufacturers that want to integrate the power of thermal imging in their product, FLIR Systems markets a full range of infrared cores. Uncooled and cooled infrared cores are available.
|
| |
|
|
| |
|
Infrared camera for other applications
There are numerous other, sometime life-saving applications for infrared cameras. Firefighters are using an infrared camera to locate people in smoke filled areas. Search and Rescue services try to locate people with the help of an infrared camera.
Any application that needs to see in total darkness, through light fog and smoke, … can benefit from the power of an infrared camera.
Browse through the site and discover the infrared camera that is best suited for your infrared application.
|
|