Japanese Simplified Chinese Español Deutsch Italia Russian Français English
 
 

Night Vision camera


A night vision camera for night vision applications

A night vision camera is being used for a wide variety of night vision applications. A night vision camera produces a clear image in the darkest of nights. A night vision camera does not need any light whatsoever to operate. A night vision camera can also see through light fog and smoke. A night vision camera produces a crisp image in practically all weather conditions.

FLIR Systems is the world leader for night vision cameras and markets a wide variety of night vision cameras that are being used for a wide variety of night vision camera applications.

Some night vision cameras are fixed mounted. Other night vision cameras are mounted on a pan/tilt. A handheld night vision camera is available. Multi-Sensor Systems, combining a night vision camera with a daylight/lowlight camera are also offered

 

 
 

 
 
Bookmark and Share

Night Vision Camera for Maritime  


A night vision camera can be installed on ships. A night vision camera can not only be installed on yachts but also commercial vessels can benefit from the power of a night vision camera. Thanks to a night vision camera, captains can navigate safely at night. A night vision camera can detect buoys, outcroppings of land, small vessels, …  A night vision camera can even detect small objects that go undetected by radar but can harm a vessel severely. A night vision camera can complement radar.

 

Night Vision Camera for Commercial Security  


Security professionals are using the power of a night vision camera to see in the darkest of nights.
A night vision camera can compliment and complete a security camera network. A night vision camera is providing the power to see threats invisible to the naked eye, turning night into day. A night vision camera make images from the heat energy that is around us all the time, not from reflected visible light, giving you true 24/7 imaging capability without lights or illuminators.

 

 

 


 

Night Vision Camera for Border Surveillance


A night vision camera is widely used for Homeland Security. Thanks to the ability of a night vision camera to detect human-sized targets several kilometers away, a night vision camera is extremely suited for border surveillance and protection. Some FLIR Systems night vision cameras can detect human-sized targets at a distance of practically 20 kilometers away.

 

 

Night Vision Camera for Law enforcement


A night vision camera is widely used by law enforcement officers worldwide. A night vision camera gives them the ability to see without being seen. For this application FLIR Systems not only markets a fixed mounted night vision camera but a handheld night vision camera as well.
 A night vision camera can help border control professionals to meet the demands they face at night and in other low-light situations. A night vision camera can be integrated in a border security project with radars and other sensors in a so called “slew-to-cue” mode.
   

Night Vision Camera for Automotive


A night vision camera can be incorporated in cars, busses, trucks, trains, … for driver vision enhancement. A night vision camera sees up to 5 times further than headlights. Thanks to a night vision camera the driver can see pedestrians and obstacles on the road from a further distance. This way a night vision camera can help to avoid deadly accidents.
   

Night Vision Camera for Aviation


FLIR Systems also markets a night vision camera that have been especially developed for aviation applications. Mounted on an aircraft, a night vision camera can be used for pilot vision enhancement.

 

     
Homepage Button - Cores
 

Night Vision Camera for Cores and components


A night vision camera have become increasingly popular the last years, Thanks to an increase in volume, the price of a night vision camera has come down. Today, more and more manufacturers are interested in integrating a night vision camera in their own product. For OEM manufacturers that want to integrate the power of a night vision camera in their product, FLIR Systems markets a full range of night vision camera cores. Uncooled and cooled night vision camera cores are available.

 
 

Night Vision Camera for other applications
There are numerous other, sometime life-saving applications for a night vision camera. Firefighters are using a night vision camera to locate people in smoke filled areas. Search and Rescue services try to locate people with the help of a night vision camera.

Any application that needs to see in total darkness, through light fog and smoke, … can benefit from the power of a night vision camera.

 

Browse through the site and discover the night vision camera that is best suited for your night vision camera application.

 
 

  © 2010 FLIR Systems. All rights reserved. Privacy Policy. Copyright Policy. Terms of Use.