Japanese Simplified Chinese Español Deutsch Italia Russian Français English
 
 

Thermal Imaging


Thermal imaging for night vision applications

A thermal imaging is being used for a wide variety of night vision applications. You do not need any light whatsoever with thermal Imaging. Thermal Imaging allows you to see in light fog and smoke. Thermal imagers produce a crisp thermal image in practically all weather conditions.

FLIR Systems is the world leader for cameras that produce a thermal image and markets a wide variety of cameras that produce a thermal image. A thermal image is being used for a wide variety of infrared applications.

Some thermal imagers produce that produce a thermal image are fixed mounted. Other thermal imagers are mounted on a pan/tilt. Handheld thermal imagers are available. Multi-Sensor Systems, producing a thermal image and a daylight/lowlight image are also offered.

 

 
 

 
 
Bookmark and Share

Thermal Imaging for Maritime  


A camera producing a thermal image can be installed on ships. Yachts but also commercial vessels can benefit from the power of a thermal image. Thanks to a thermal image, captains can navigate safely at night.  A thermal image can detect buoys, outcroppings of land, small vessels, … A thermal image can even detect small objects that go undetected by radar but can harm a vessel severely. A thermal image can complement radar.

   

Thermal Imaging for Commercial Security  


Security professionals are using the power of a thermal image to see in the darkest of nights.
A thermal image can compliment and complete a security camera network. A thermal images is providing the power to see threats invisible to the naked eye, turning night into day.  A thermal image is produced from the heat energy that is around us all the time, not from reflected visible light, giving you true 24/7 thermal imaging capability without lights or illuminators.

 

 

 

 

Thermal Imaging for Border Surveillance


Thermal imaging is widely used for Homeland Security. Thanks to the ability of a thermal image to detect human-sized targets several kilometers away, a thermal image is extremely suited for border surveillance and protection. A FLIR Systems thermal image can detect human-sized targets at a distance of practically 20 kilometers away.

A thermal image can help border control professionals to meet the demands they face at night and in other low-light situations. A camera that produces a thermal image can be integrated in a border security project with radars and other sensors in a so called “slew-to-cue” mode.

   
 

Thermal Imaging for Law enforcement


A thermal image is widely used by law enforcement officers worldwide. A thermal image gives them the ability to see without being seen. For this application FLIR Systems not only markets fixed mounted camera that produce a thermal image but handheld cameras that produce a thermal image as well.
 
   

Thermal Imaging for Automotive


A thermal image can be incorporated in cars, busses, trucks, trains, … for driver vision enhancement. A thermal image sees up to 5 times further than headlights. Thanks to a thermal image the driver can see pedestrians and obstacles on the road from a further distance. This way a thermal image can help to avoid deadly accidents.
   

Thermal Imaging for Aviation


FLIR Systems also markets cameras that produce a thermal image that have been especially developed for aviation applications. Mounted on an aircraft, a thermal image can be used for pilot vision enhancement.
     
Homepage Button - Cores  

Thermal Imaging for Cores and components


Thermal imaging has become increasingly popular the last years, Thanks to an increase in volume, the price of cameras that produce a thermal image has come down. Today, more and more manufacturers are interested in integrating a camera that produce a thermal image in their own product. For OEM manufacturers that want to integrate the power of a thermal image in their product, FLIR Systems markets a full range of cores that produce a thermal image. Uncooled and cooled infrared cores that produce a thermal image are available.

 
 

Other applications for Thermal imaging
There are numerous other, sometime life-saving applications for a thermal image. Firefighters are using a thermal image to locate people in smoke filled areas. Search and Rescue services try to locate people with the help of a thermal image.

Any application that needs to see in total darkness, through light fog and smoke, … can benefit from the power of a thermal image.

 

Browse through the site and discover the camera that produces a thermal image that is best suited for your thermal imaging application.

 
 

  © 2011 FLIR Systems. All rights reserved. Images/content for illustration purposes only. Privacy Policy. Copyright Policy. Terms of Use. 
Pan tilt FLIR Motion Control Systems