Detect Benzene, an Important Petrochemical Building-Block

Benzene is an elementary petrochemical derived from crude oil that’s notable for its sweet smell. Benzene has a high octane number, making it an important fuel additive to gasoline. It’s also used in the production of heavy chemicals, lubricants, and plastics. Breathing in high levels of benzene can be fatal, and long term exposure can cause cancer.

Get a FREE Copy of FLIR's new iBook:

Optical Gas Imaging: The Professional Guide

 

Gain a greater understanding of optical gas imaging (OGI) technology and how it can help you find and repair gas leaks quickly, saving time, money, and the environment. This new iBook offers:

  • In-depth look at industry applications
  • Rich video content
  • Details on how OGI and infrared work
  • Expert tips for maximizing OGI surveys
From application stories to videos of fugitive emissions, this iBook has everything you need to understand OGI.

Get the
iBook Now!
 

OGI Application Stories

T820591

Remote Detection and Localization of Gas Leaks with Autonomous Mobile Inspection Robots in Technical Facilities

Detection of gas leaks in industrial facilities is not only dangerous and time-consuming: it is also susceptible to human error and interpretation. In order to provide a safer, more efficient and more reliable detection solution, RoboGasInspector was conceived. This innovative robot system for remote detection and localization of gas leaks was developed by a range of German companies and institutes, and uses a FLIR GF320 optical gas imaging camera.

Read Application Story  

T820370

Environmental Protection with a FLIR OGI Camera

Some industrial, pharmaceutical and petrochemical plants emit gases that can harm the environment and impede the health of company employees and inhabitants of the surrounding area. Environmental protection agencies have the responsibility to make sure that these emissions fall within governmental and international policy guidelines. To help them with that task environmental protection agencies can use an optical gas imaging camera.

Read Application Story  

Optical Gas Imaging Cameras for Benzene Leak Detection

 

Handheld: FLIR GFx320

Ground breaking technology for visualizing fugitive leaks.

Explore  


Handheld: FLIR GF300/GF320

Detect benzene leaks from production plants, or spot non-functioning benzene flares.

Explore  


Fixed: FLIR G300a

Provides continuous monitoring of flares, allowing energy producers to immediately spot if a flare is out and benzene is leaking.

Explore  

What Our Customers Have to Say

 

Customer Survey verified by TechValidate.

 
 

Customer Evidence verified by TechValidate.