Detecting Flammable Hydrocarbons for Fuel or Propellants

Propane also has agricultural and manufacturing applications, while butane is used as a fuel additive, an accelerant, a refrigerant, and a component of other chemicals. Leaks of either chemical can cause explosions. The ability to detect fugitive emissions from faulty valves, storage, and transport systems – and to do so from a safe distance – is therefore critical.

Get a FREE Copy of FLIR's new iBook:

Optical Gas Imaging: The Professional Guide

 

Gain a greater understanding of optical gas imaging (OGI) technology and how it can help you find and repair gas leaks quickly, saving time, money, and the environment. This new iBook offers:

  • In-depth look at industry applications
  • Rich video content
  • Details on how OGI and infrared work
  • Expert tips for maximizing OGI surveys
From application stories to videos of fugitive emissions, this iBook has everything you need to understand OGI.

Get the
iBook Now!
 

OGI Application Stories

Environmental protection with a FLIR optical gas imaging camera

Some industrial, pharmaceutical and petrochemical plants emit gases that can harm the environment and impede the health of company employees and inhabitants of the surrounding area. Environmental protection agencies have the responsibility to make sure that these emissions fall within governmental and international policy guidelines. To help them with that task environmental protection agencies can use an optical gas imaging camera.

Read Application Story

FLIR optical gas imaging camera helps improve environment and safety at Borealis Stenungsund

Many petrochemical plants handle invisible gaseous hydrocarbons. Most of these gases pose some sort of safety aspects. They may be toxic, or can cause health issues in case of long term exposure. Others are highly flammable, explosive even, and most of them will have a negative impact on the environment if they enter the atmosphere in large quantities. That is why leak detection is of vital importance in these petrochemical plants.

Read Application Story

Ten tips to get the most out of your OGI Camera

Optical Gas Imaging (OGI) cameras use spectral wavelength filtering and Sterling cooler cold filtering technology to visualize the infrared absorption of VOC/hydrocarbon, SF6, refrigerants, carbon monoxide and other gases whose spectral absorption matches the response of the camera.

Read Application Story

Optical Gas Imaging Cameras for Propane / Butane Leak Detection

 

Handheld: FLIR GFx320

Intrinsically safe OGI camera for visualizing fugitive leaks at natural gas well sites, off-shore platforms, liquid natural gas terminals, and more.

Explore


Handheld: FLIR GF300/GF320

This preventative maintenance solution spots leaks nine times faster than traditional "sniffer" methods.

Explore


Fixed: FLIR G300a

Provides continuous monitoring of oil and gas field components, allowing energy producers to immediately spot dangerous gas leaks and repair them quickly.

Explore


Fixed: FLIR A6604

These cameras provide excellent coverage of remote areas, or components that are difficult to access.

Explore

What Our Customers Have to Say

 

Customer Survey verified by TechValidate.