This product has been discontinued. Take a look at our current Analog Dome Varifocal cameras.
DBD24TL

DBD24TL Dome Camera

Ultra Resolution Varifocal IR Dome Camera

The FLIR Summit Series DBD24TL Varifocal IR Dome Camera provides dependable performance in indoor environments with 600TVL Ultra Resolution plus a 2.8-12mm varifocal lens. The built-in mechanical IR cut filter ensures accurate color reproduction by preventing discoloration caused by infrared lighting when visible light is present. When conditions change to low-light, infrared light from the built-in LED’s is utilized to render a clear image up to 65ft. DBD24TL is an ideal economical option for indoor applications such as offices or retail environments.