FLIR Infrared Building Cameras


INFRARED CAMERAS FOR BUILDING INSPECTIONS AND DIAGNOSTICS

 

 

Residential, commercial, and industrial buildings can all suffer from a wide variety problems associated with their design, construction, equipment failures, and external forces. These problems can result in large expenditures to fix things that have gone unnoticed for too long. Even when symptoms are evident, it's often difficult to find the source of the problem. This can result in secondary damage that poses risks to occupants, or leads to destruction of the building. FLIR B-Series infrared cameras are a non-invasive way for inspectors and contractors to quickly find problems and initiate repairs. 

 

 

Infrared (IR) thermography with FLIR cameras is a non-contact method for detecting the difference in temperature between a problem area and its surroundings. Depending on the underlying cause, the problem area may be warmer or colder than its surroundings. This temperature difference is clearly visible in the camera's image display. A trained operator can immediately home in on the source of the problem and what's causing it – without having to first tear into walls or disassemble equipment.

 

The FLIR B-Series infrared cameras are excellent tools for Building Diagnostics, Energy Audits, Moisture Detection, Restoration & Remediation, HVAC and plumbing, as well as for Property and Facility Maintenance.

FLIR Simplifies Your Work

FLIR's advanced IR cameras are preferred by building experts for fast, reliable, accurate building diagnosis for the entire range of building problems. FLIR also offers building diagnostics training for a fast payback on your investment. Learn the art and science of using an IR camera as a non-invasive inspection and reporting tool. Take the new online Building IR Basics class offered by the Infrared Training Center (ITC) or one of their other certified IR classes.

Download Product Literature

 B400 infrared camera 

Compare models

Find your FLIR B-Series model
Learn More

 

Related industries

Building

Building

An infrared inspection locates poor insulation causing unnecessary energy leaks.

Baixe o Livro Gratuitamente

12 Things to Know Before Buying an Infrared Camera

12 Pontos Que Você Precisa Saber Antes de Comprar uma Câmera Infravermelha.
Fazer o download

Get the FLIR Science Camera FOV Calculator

FLIR Science Camera FOV Calculator

Want the FOV calculator FLIR's Dave Bursell discussed in his "IR Camera Measurement and Microscopy" webinar? Download it now

Home Inspection Video

Insulation Video 

FLIR infrared cameras find gaps in insulation during home inspections and energy audits.

Watch Now