FLIR ThermaTrak™
Revolutionary Technology to Locate Lost, Stolen or Missing Infrared Cameras
ThermaTrak™, an exclusive new high-tech service to locate missing or stolen infrared cameras and thermal imagers is now being included in several models of FLIR cameras. This breakthrough technology employs recovery software that pinpoints the geographic location of the lost, stolen or missing infrared camera. Additionally, the ThermaTrak software embedded in the camera tracks the IP address, hostname, and even the Internet service provider (ISP) being used after the IR camera has gone missing or been stolen and is connected to the Internet.
This revolutionary new application can also be used by companies as an asset management tool when they have multiple cameras in the field. Companies receive emails with updated location reports each time the IR camera is connected to a computer with internet access.
This is a low cost way to give added protection to your investment in IR. Call today, 800 GO INFRA (464 6372), for more information.