Battery Energy Storage Systems

Why FLIR thermal imaging cameras are the optimal choice for early fire detection at BESS sites

Battery Energy Storage Systems (BESS) are essential components of today's energy infrastructure, facilitating the storage and distribution of electricity to effectively balance supply and demand and ensure grid stability. Typically housed in large, outdoor containers containing stacks of battery cells, these battery systems are becoming safer, more stable, and more reliable with each generation.

There is still the potential for critical temperature fluctuations that could lead to fires. Vigilance is vital, as are thermal sensor systems designed to detect signs of damage or failure that often preceed fires.

What is the safety concern?

Battery site operators are particularly concerned with thermal runaway, which can occur when temperatures in a battery cell suddenly spike and spread to other cells, potentially leading to fires and the release of harmful gases. Given how tightly packed these units are, just one overheating due to a fault, damage, or impact can create a devastating cascade within the unit wiping out all assets in a fire that can last for days.

BESS Site Fires Demonstrate that Vigilance is Vital

Several incidents at BESS sites in 2024-2025 underscore the fundamental requirement for robust monitoring for thermal runaway. For example, a sizable fire broke out at the Vistra energy storage facility near Santa Cruz, California in January 2025. 

The fire released toxic gases, forcing the evacuation of 1500 residents. And it was challenging to extinguish due to the nature of lithium-ion batteries, which may explode when brought into contact with water and can reignite in high temperatures. Among the toxic gases that can be released in a BESS fire is hydrogen fluoride gas, which the US Centers for Disease Control and Prevention lists as an irritant to the eyes, nose, mouth, throat, and lungs.


 

Why BESS Site Owners Need Flir Thermal Imaging Solutions

To mitigate the risks to BESS facilities, Flir offers state-of-the-art thermal imaging cameras that are customizable to site size and complexity, offer open platforms for easy integration, and include built-in software for advanced thermal analysis and alarms on potential hot spots.

FH-Series™ R PTZ

Pan-Tilt Thermal Security Cameras

FH-Series™ R PTZ

Multi-Spectral Pan-Tilt-Zoom Camera for Fire Detection and Monitoring of Surface Temperature Thresholds

FLIR A500f/A700f Advanced Smart Sensor

Smart Cameras in Enclosures

FLIR A500f/A700f Advanced Smart Sensor

Fixed-Mount Thermal Imaging Camera for Condition Monitoring and Early Fire Detection

FLIR A50/A70 Smart Sensor

Smart Camera Solutions

FLIR A50/A70 Smart Sensor

Fixed-Mount Thermal Camera

 

Flir Early Fire Detection for BESS in Action

Tech Note

What Are the Inherent Risks of BESS Sites, and How Can Operators Overcome Them?

Read more
Tech Note

Why a Surge in Battery Energy Storage System Installations is Set to Supercharge Global Infrastructure

Read more
Tech Note

Ensuring Safety and Preventing Fire with Flir Thermal Monitoring for Battery Energy Storage Systems

Read more