Teledyne FLIR OEM Launches Prism SKR Automated Targeting and Homing Software

Prism SKR addresses the ever-growing need for autonomously guided weapon systems: low-cost missiles, loitering munitions, and one-way drones

 

Goleta, CA, March 18, 2025 – Teledyne FLIR OEM, part of Teledyne Technologies Incorporated (NYSE:TDY), today announced Prism™ SKR,

the newest addition to the Prism embedded software ecosystem. Prism SKR, pronounced “seeker,” sets a new standard in precision automatic target recognition (ATR) for autonomously guided weapon systems, including loitering munitions, air-launched effects (ALE), counter-unmanned aerial systems (C-UAS), low-cost missiles, and smart munitions.

Prism SKR operates seamlessly at the edge on low-power embedded processors. Compatible with both infrared (IR) thermal and visible camera data, Prism SKR's advanced algorithms provide real-time target position, identification, direction of motion, and aim-point localization. The target information is used to guide the platform's autonomous flight system for air-to-ground (A2G), ground-to-air, air-to-air, and ground-to-ground operations.

“Compatible with existing autonomy and navigation software via a Weapon Open System Architecture (WOSA) compliant interface, Prism SKR represents a significant leap forward in autonomous precision target detection, identification, and tracking technology for defense OEM developers and integrators,” said Dan Walker, vice president of product management, Teledyne FLIR OEM. “Additionally, developers can reduce development risk and costs with plug-and-play integration with the Prism embedded software ecosystem and Teledyne FLIR IR camera modules.”

The Prism software ecosystem streamlines development and shortens time to market with out-of-the-box compatibility. Starting with the Prism AI embedded software, developers and integrators can utilize detection and tracking models leveraging Teledyne FLIR OEM's six million visible and thermal annotations. Custom target lists can quickly be incorporated using the Prism AIMMGen synthetic dataset and model training tool chain. Finally, Prism Supervisor empowers autonomous mission control and platform guidance with Prism SKR, where ATR is required.

With its advanced features, robust ecosystem, and a complete application programming interface (API) and software development kit (SDK) for customization and performance optimization, Prism SKR is the ultimate solution for OEMs seeking to enhance the precision and reliability of autonomous weapon systems.

For more information about Prism SKR and the Prism family of embedded software, please visit www.flir.com/prism. Teledyne FLIR OEM will show Prism at SPIE Defense + Commercial Sensing in Orlando, Florida, April 13-17, 2025.

 

About Teledyne FLIR

Teledyne FLIR OEM, a Teledyne Technologies company, is a world leader in intelligent sensing solutions for defense and industrial applications, with approximately 4,000 employees worldwide. Founded in 1978, the company creates advanced technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.teledyneflir.com or follow @flir.

Related Articles