Recoverable Loitering Munitions Are More Cost-and Mission-Effective Than One-Way Attack Drones, Says New Teledyne FLIR Defense Whitepaper

/globalassets/news/news-center/government--defense/loitering-munitions-white-paper-social-media-image-1200x628-v3.jpg

Recoverable and reusable loitering munition solutions are set to significantly alter the modern battlespace as ground units seek to dominate the ‘atmospheric littoral’

WASHINGTON, D.C, April 28, 2025 ― In a new whitepaper, Teledyne FLIR Defense, part of Teledyne Technologies Incorporated (NYSE:TDY), says that emerging cost-effective precision strike solutions that can be safely recovered and reused offer a strong alternative to more commonly deployed ‘One-Way Attack’ or First Person View (FPV) drones.

In the new paper, USE IT, DON’T LOSE IT: The Case for Recoverable and Reusable Loitering Munitions, FLIR Defense argues that newer, advanced loitering munition unmanned aircraft systems (LMUAS) are better suited to support operations in the ‘atmospheric littoral.’ An emerging strategic concept, the atmospheric littoral describes the very low-altitude airspace (up to several hundred feet above ground level) which, if controlled, can significantly enhance the ground maneuver of combat units.

The paper highlights the total ownership cost of FPV and legacy loitering munitions currently on the market. Most systems are single use, so whether they successfully hit a target or not, they are a spent cost. These types of munitions are more expensive and complicated to train with, operate, and maintain, compared to recoverable LMUAS that can be safely brought back if target conditions change, or fitted with an inert payload for training exercises.

The whitepaper also explains how newer recoverable LMUAS, such as the FLIR Defense Rogue 1™, can deliver greater precision strike capability to warfighters at the tactical edge. Rogue 1’s patented gimballed warhead allows users to ‘point’ and deliver its munitions far more accurately, so that the lightweight system can disable armored platforms by targeting vulnerable spots on the vehicle. Increased precision makes up for the reduced payload capacity of the VTOL airframe compared to larger, fixed-wing platforms that can deliver heavier payloads but with less accuracy.

“Recoverable LMUAS offer small fighting units a big advantage when they can train more efficiently, deliver precision effects on the battlefield, and yet be able to reuse a system when target conditions change up to the last second,” said Dave Viens, vice president of US Business Development at Teledyne FLIR Defense. “As our ‘Use it, Don’t Lose It’ whitepaper points out, the atmospheric littoral has quickly become the key battlespace warfighters must control – and dominate – to defeat our enemies in modern conflicts.

“We believe the critical technologies embodied in the Rogue 1 lethal UAS offer distinct advantages to traditional ‘one-way’ FPV drones, giving combat units the edge they need to control the atmospheric littoral,” Viens added.

Other key points in the paper include:

  • ‘One-Way Attack’ and ‘First Person View’ drones often suffer from major operational disadvantages across the battlespace, particularly in terms of cost, training, use case DEV/OPS, lethal effect, and precision.
  • Recoverable and reusable loitering munitions not only reduce capital expenditure and training cycles but also optimize mission success.
  • Military-grade quadrotor loitering munitions equipped with state-of-the-art fuzing solutions and precision payloads are ideally suited to satisfy emerging demand signals at the tactical edge.
  • Next-generation technologies, including ML/AI tools such as Aided Target Recognition (AiTR), will open up more possibilities for loitering munitions in the near future.

Click here to download the new Teledyne FLIR Defense whitepaper, USE IT, DON’T LOSE IT: The Case for Recoverable and Reusable Loitering Munitions.

# # # #

About Teledyne FLIR Defense

Teledyne FLIR Defense has been providing advanced, mission-critical technology and systems for more than 45 years. Our products are on the frontlines of the world’s most pressing military, security and public safety challenges. As a global leader in thermal imaging, we design and build sophisticated surveillance sensors for air, land and maritime use. We develop the most rugged, trusted unmanned air and ground platforms, as well as intelligent sensing devices used to detect chemicals, biological agents, radiation and explosives. At Teledyne FLIR Defense we bring together this expertise to deliver solutions that enable critical decisions and keep our world safe – from any threat, anywhere. To learn more, visit us online or follow @flir.

About Teledyne Technologies

Teledyne Technologies is a leading provider of sophisticated digital imaging products and software, instrumentation, aerospace and defense electronics, and engineered systems. Teledyne's operations are primarily located in the United States, the United Kingdom, Canada, and Western and Northern Europe. For more information, visit Teledyne's website at www.teledyne.com.

 

Related Articles