Configuration

Do you have a general specification for the power input/output requirements of the A320 & A325?

Learn more

Instructions

Does FLIR offer an SDK to control and get video stream from the FLIR IR cameras?

Learn more

Technical Guidance

Can I control the A320 or A325 (A320G) camera using serial communication, RS-232?

Learn more

System Requirements

Which lens alternatives can I get with A310, A320, A315 and A325 (A320G)?

Read the Story

Configuration

What is the array size of the detector in the A320 and A325 (A320G)?

Read the Story

Technical Guidance

Are cameras such as the X6900SC / X6800SC / X8500SC fully GeniCam compliantl?Are there any restrictions (maximum framerate, superframing, preset sequencing) in doing so, or is it full control?

Learn more

Warranty & RMA

FLIR Standard Warranty

Learn more

Technical Guidance

How can I connect my FLIR Ethernet camera to FLIR Tools?

Read the Story

Compatibility

Which FLIR cameras are supported by the Atlas SDK?

Read the Story

Instructions

I see that there are two firmware versions for the A3xx cameras. Which one should I choose?

Read the Story