Configuration
How do I configure Explicit Messages to pull data from the FLIR AX8 or A310 camera?
Read the StoryConnectivity
How do I connect to my FLIR AX8 to a computer? What IP address should I use?
Read the StoryApplication Note
Set Up a Local Mail Server and Receive Email When an Alarm is Triggered
Read the StoryTechnical Guidance
How do I work with alarms on the FLIR AX8 using the digital output and input?
Read the StoryInstructions
How do I configure my FLIR AX8 to send an e-mail every time an alarm goes off if I don't have access to a local E-mail server?
Read the StorySystem Requirements
How many images/videos can the FLIR AX8 store in its internal memory?
Read the StoryUse Case Scenario
Why Yacht Owners Are Adding Thermal Imaging Cameras to Minimise the Risk of Lithium-Ion Battery Fires
Read the StoryTechnical Guidance
How do I enable/disable pre-configured alarms on FLIR A310 and AX8 cameras using a PLC?
Learn more