I like to add several areas to measure the temperature. How many areas can I define using the camera built-in software?
The cameras with built analysis can have this many areas and spots:
Camera | Areas | Spots |
A20, A40, A320 | 4 | 4 |
A310 | 10 | 10 |
AX8 | 6 | 6 |
A20, A40 and AX8 are set up using buttons on the camera or the Web interface. To set up the A320 or A310, use the IR Monitor utility.