Ladybug SDK
This is the latest version of the Ladybug SDK which supports Ladybug2, Ladybug3, Ladybug5, and Ladybug5+. The initial Linux version of the Ladybug library supports both 1394 and USB3 cameras on Ubuntu 16.04 (both x86 and x86_64). The initial Linux SDK focuses on image acquisition, stream recording and GPS support via a command line application (LadybugRecorderConsole).