Can the Ladybug SDK stitch fewer than six images?
Last Revision Date: 4/20/2015
This article explains that the Ladybug SDK is not currently configured to perform stitching on fewer than six images.
ANSWER:
The Ladybug SDK is not currently configured to perform stitching on fewer than six images.
The on-camera image buffer receives images from all six sensors. The SDK cannot disable some of the six images to increase the frame rate.
If stitching performance is a concern, make sure the graphics card has OpenGL support and the stitching is hardware accelerated. For more information, refer to the SDK example program ladybugPanoStitchExample.