Camera Software

FLIR Camera Controller GUI for Vue, Tau and Quark

The FLIR Camera Controller Graphical User Interface (GUI) is a Windows 7 and later PC program that enables remote command and control of Vue, Tau 2 or Quark 2 functions and features through a USB or RS-232 serial interface to the camera. IMPORTANT: Make sure there is only one version of the GUI installed at a time on your computer. If you intend to upgrade from an older version of GUI to a newer version, be sure to completely uninstall the older version first by using the Add or Remove Programs function of the Control Panel in Windows.

FLIR Camera Controller GUI for Vue, Tau & Quark - v118 (.zip)

If you are using the Video, Power, Communication (VPC) accessory with Vue, Tau or Quark, the first time you connect to the camera via USB you will need to know the COM port number. Installing the GUI will enable a Silicon Labs driver. The USB COM port number for Vue / Tau / Quark can be found by opening the Device Manager, then expand the Ports icon. In the example below, COM6 has been identified as the USB COM port. The actual COM port may be different on the PC being used.


FLIR Universal Camera Controller GUI for Tau SWIR

The FLIR Universal Camera Controller Graphical User Interface (GUI) is a PC program that enables remote command and control of Tau SWIR functions and features through a USB or Camera Link serial interface to the camera. The Universal Camera Controller GUI Software is compatible with all versions of the Tau SWIR camera (25um and 15um all versions). IMPORTANT: This GUI and the "FLIR Camera Controller GUI" that is generally used with the Tau and Quark Infrared cameras are NOT interchangeable. The use of the improper GUI can render the camera inoperable and the camera must be returned to the factory for repair.

FLIR Universal Camera Controller GUI for Tau SWIR (.zip)