Press release

 


FLIR Systems launches new FLIR E30

Visual camera integrated and extended temperature range

After the successful introduction of the FLIR E-Series in 2011, FLIR Systems is now launching an improved model of the FLIR E-Series entry model: FLIR E30.

 

Visual camera incorporated

The new FLIR E30 is now equipped with a visual camera. A visual image is often used as a reference against the thermal image. It clearly shows the people that need to do the actual repair where the problem is exactly located.

 

The visual camera produces 2 Megapixel images.

 

By pressing only one button the camera stores the thermal image and the visual image simultaneously. A LED-lamp installed on the front of the camera assures that good quality visual images can also be taken in darker environments. Just like all FLIR E-Series, the FLIR E30 is equipped with a laser pointer that will help the user to associate the hot spot on the thermal image with the real physical target in the field.

 

Extended temperature range

The FLIR E30 is equipped with a state-of-the-art uncooled Vanadium Oxide microbolometer detector that produces clear thermal images of 160 x 120 pixels. Temperature differences as small as 0.1˚C become clearly visible on a crisp thermal image.

 

The new FLIR E30 can measure temperatures between -20˚C and +350˚C.

 

Rugged and easy-to-use

The FLIR E30 is rugged to face everyday use in the most harsh environments. The vital inner core is well protected (IP54 rated). Extremely easy-to-use, all buttons for controlling the FLIR E30 are right underneath your fingertips. The large 3.5" LCD touchscreen shows clear thermal images and allows access to all camera features.

 

FLIR Tools included

Every FLIR E-Series thermal imaging camera comes with FLIR Tools software.

 

FLIR Tools allows to import thermal images directly from the FLIR E-Series to a PC and for basic reporting and analysis of your findings.

 

Main features of FLIR Tools are:

 

  • Import images from the thermal imaging camera to a PC
  • Lay out, move and resize measurement tools on any thermal image
  • Create PDF imagesheets of specific images
  • Add headers, footers, and logos to reports
  • Apply filters when searching for images

Users that need more reporting functionalities can choose for FLIR Reporter software which is also compatible with the new FLIR E-Series.

 

About thermal imaging

Thermal imaging is the use of cameras constructed with specialty sensors that “see” thermal

 

energy emitted from an object. Thermal, or infrared energy, is light that is not visible to the human

 

eye because its wavelength is too long to be detected. It’s the part of the electromagnetic spectrum

 

that we perceive as heat. Infrared allows us to see what our eyes can not. Thermal imaging cameras produce images of invisible infrared or “heat” radiation. Based on temperature differences between objects, thermal imaging produces a clear image. It is an excellent tool for predictive maintenance, building inspections, research & development and automation applications. It can see in total darkness, in the darkest of nights, through fog, in the far distance, through smoke. It is also used for security and surveillance, maritime, automotive, firefighting and many other applications.

 

About FLIR Systems

FLIR Systems is the world leader in the design and manufacturing of thermal imaging cameras for

 

a wide variety of applications. It has over 50 years of experience and thousands of thermal imaging

 

cameras currently in use worldwide for industrial maintenance, building inspections, research &

 

development, security and surveillance, maritime, automotive and other night-vision applications.

 

FLIR Systems has eight manufacturing plants located in the USA (Portland, Boston, Santa Barbara

 

and Bozeman), Stockholm, Sweden, Talinn, Estonia and near Paris, France. It operates offices

 

in Australia, Belgium, Brazil, China, Dubai, France, Germany, Hong Kong, Italy, Japan, Korea, the

 

Netherlands, Russia, Spain, UK and the USA. The company has over 3,200 dedicated infrared

 

specialists, and serves international markets through an international distributor network providing

 

local sales and support functions.

 

More about FLIR Systems and our products can be found at www.flir.com

 

FLIR Commercial Systems B.V.

Marieke Kers

PR & Advertising Manager EMEA

Charles Petitweg 21

4847 NW Breda

The Netherlands

Phone : +31 (0) 765 79 41 94

Fax : +31 (0) 765 79 41 99

e-mail: flir@flir.com