Online FoV Calculators
Online FoV Calculators
Updated Date
15/11/2023 04.59 PM
How to calculate the Field of View (FoV) of a camera / lens configuration?
How to calculate the Field of View (FoV) of a camera / lens configuration?
To know if a camera can measure a target at a certain distance some calculations can be done.
We have a utility called the FoV calculator which is available on this site, access it by following the procedure below:
- Go to Download Datasheet and select a camera series
- Click the FoV Calc. hyperlink for a camera–lens combination. This displays the FoV calculator.
- To select a different camera–lens combination for a particular camera, select the new combination in the drop-down menu.
The FoV calculator displays the following results:
- HFOV: horizontal field of view in meters and feet.
- VFOV: vertical field of view in meters and feet.
- Depth of field—far limit in meters and feet.
- Depth of field—near limit in meters and feet.
- IFOV: instantaneous field of view in millimeters and inches.
- Distance to target in meters and feet.
Tips
- Each camera may have interchangeable lenses. If this is the case, you can choose a lens from the drop down menu.
- You can switch between metric or imperial units using the drop-down menu.
- Type in several distances separated by commas to calculate the FoV at all desired distances.
Example for an A655sc 45°
Go to camera datasheets and select the product:
Select the 45° lens from the dropdown menu:
Type in the desired distance to calculate the FoV or use the listed default values.
The FLIR Advantage