FLIR has received third party validation that the FLIR GF300 and GF320 cameras are compliant with the following sensitivity standard laid out by the EPA in the NSPS OOOOa Methane rule:

Your optical gas imaging equipment must be capable of imaging a gas that is half methane, half propane at a concentration of 10,000 ppm at a flow rate of ≤60g/hr from a quarter inch diameter orifice.

LEARN MORE ABOUT THE IMPLICATIONS OF METHANE EMISSIONS

Watch FLIR VP of US Sales, Brent Lammert's, technology brief to the Environmental and Energy Study Institue (EESI) on reducing methane emissions with optical gas imaging.

Watch Video

FLIR WORKS TO SUPPORT OIL & GAS CUSTOMERS FACING NEW EPA METHANE RULE

With the June 3rd Federal Register publication of the Environmental Protection Agency’s new methane standard comes a host of new concerns for the Oil and Gas industry.

Read More

Optical Gas Imaging and Furnace Inspection

Find industrial gases and chemical compounds faster and better with FLIR.

Get a FREE Copy of FLIR's new iBook:

Optical Gas Imaging: The Professional Guide

Gain a greater understanding of optical gas imaging (OGI) technology and how it can help you find and repair gas leaks quickly, saving time, money, and the environment. This new eBook offers:

  • In-depth look at industry applications
  • Rich video content
  • Details on how OGI and infrared work
  • Expert tips for maximizing OGI surveys
From application stories to videos of fugitive emissions, this eBook has everything you need to understand OGI.

Get the
iBook Now!


Find the infrared camera that's right for you:

FLIR GF300/320

FLIR GF300/320

FLIR GF320 thermal camera is a preventative maintenance solution to spot leaks in piping, flanges and connections in petrochemical operations.

EXPLORE

FLIR GF304

FLIR GF304

The FLIR GF304 detects refrigerant gas leaks without interrupting or shutting down operations in food production, storage and retail; pharmaceutical; automotive; and air conditioning.

EXPLORE

FLIR GF306

FLIR GF306

FLIR GF306 thermal cameras detect and visualize SF6 and 25 other harmful gases quickly from a safe distance and without the need to interrupt plant production processes.

EXPLORE

FLIR GF309

FLIR GF309

These cameras are ideal for monitoring all types of furnaces, heaters and boilers, particularly in the chemical, petrochemical and utility industries.

EXPLORE

FLIR GF343

FLIR GF343

Spot CO2 leaks quickly, easily, and from a safe distance with FLIR GF343. Fast and accurate detection of CO2 leaks can be vital to safe, efficient operations with minimal down time.

EXPLORE

FLIR GF346

FLIR GF346

FLIR GF346 infrared cameras are capable of finding carbon monoxide and a number of other gases, and unbeatable for detecting even the smallest gas leaks.

EXPLORE

FLIR G300a, G300pt and A6604

Fixed OGI Cameras

FLIR's G300a, G300pt and A6604 allow you to continuously scan installations in remote or difficult to access zones and immediately be informed of dangerous or costly gas leaks.

EXPLORE

Videos

See for Yourself What You Can Do With Thermal Imaging.
Check out these videos.

FLIR Customer Success Stories -
Optical Gas Imaging Applications

FLIR regularly publishes customer success stories where you can read how our customers are using FLIR infrared cameras and thermal imaging solutions. To access more customer success stories, please visit the OGI application stories page.

Through-Flame Thermal Cameras Can Take the Heat

Through-Flame Thermal Cameras Can Take the Heat

Does your process heating operation need a fast, noncontact, nondestructive way to gather both qualitative and quantitative information to prevent or minimize downtime? Of course it does, and that is why you should consider a through-flame thermal camera. Read customer success story

Inspectahire relies on the FLIR GF320 Optical Gas Imaging camera for maintenance inspections

Inspectahire Relies on the FLIR GF320 Optical Gas Imaging Camera for Maintenance Inspections

Supported by the most advanced technologies around, Inspectahire helps its customers manage their safety, profitability and environmental impact of their assets. When the company is tasked with the detection of fugitive hydrocarbon emissions, FLIR’s GF320 Optical Gas Imaging (OGI) camera is their preferred technology to use. Read customer success story

Integral UK Helps its Customers Save Costs

Integral UK Helps its Customers Save Costs

Chillers commonly use refrigerant gas to provide cooling and therefore temperature control for large commercial properties. Integral is a maintenance specialist, who regularly maintains those assets on behalf of some of the largest clients in Great Britain, many of them household names. Read customer success story

FLIR Optical Gas Imaging Camera Helps Improve Environment and Safety at Borealis Stenungsund

FLIR Optical Gas Imaging Camera Helps Improve Environment and Safety at Borealis Stenungsund

Many petrochemical plants handle invisible gaseous hydrocarbons. These gases may be toxic, or can cause health issues in case of long term exposure. Others are highly flammable, explosive even, and most of them will have a negative impact on the environment if they enter the atmosphere in large quantities. That is why leak detection is of vital importance in these petrochemical plants. Read customer success story