Thermal Imaging for Energy Auditing & Home Inspection

 

Air tightness and thermal imaging testing are important quality control measures when building or renovating a house. Heat losses in buildings can account for up to 50% of the total energy consumption and comes from air leakage through chimneys, attics, wall vents and badly sealed windows/doors, etc.

 

  

 

All new buildings must meet air tightness requirements of the Building Regulations. By reducing air leakage, you obtain a better comfort in the building. The building can also be heated more efficiently to conserve energy and save money.

Detection and Visualization of Air Infiltration and Exfiltration

Adequate air exchange is essential for occupants' health and safety, but most buildings have a far higher rate of air exchange than is necessary. The root cause is often poor design and/or construction which allows air leakage from the inside or outside of the building, or the opposite. The leakage pathway is often complex and, without thermal imaging, extremely difficult to visualize. This also allows the contractors to quickly identify and repair the problem areas to stop the energy loss immediately.

 

Improved Energy Efficiency

To identify areas of energy waste, infrared imaging has quickly become a valued tool in identifying problems related to energy loss, missing insulation, inefficient HVAC systems, radiant heating, water damage on roofs, and much more. A thermal imaging camera identifies patterns of heat loss that are invisible to the naked eye. Thermal imaging quickly indicates the air leaks within a property and measurement data are easily compiled into a report.

 

Professional home inspectors and energy auditors are using leading-edge infrared technology from FLIR to perform energy auditing of homes and buildings to improve energy efficiency, thus leading to savings on energy costs.

 

Choose the infrared camera that is right for you:


FLIR i-Series Infrared Camera


FLIR i3, i5 & i7 Infrared Cameras

Starting at only $1,195, FLIR i-Series point and shoot thermal cameras are easy-to-use, lightweight, and very affordable – the most cost-effective way to add infrared images and temperature data to any toolbox.

FLIR E-Series Infrared Camera



FLIR E30bx - E60bx Infrared Cameras

The fast and powerful new FLIR E-Series bx is revolutionizing the way compact, professional thermal cameras capture, analyze and share images and data. Featuring touchscreen tools and Wi-Fi connectivity.

FLIR T-Series bx Infrared Camera

FLIR T420 bx and T440 bx Infrared Cameras

Flexible FLIR T-Series bx high-performance cameras feature superior thermal resolution and an ergonomic rotating optical block that helps you capture shots from tough angles comfortably, and now include Wi-Fi connectivity to mobile devices.

FLIR T-Series bx Infrared Camera

FLIR T620 bx and T640 bx Infrared Cameras

The innovative FLIR T620 bx and FLIR T640 bx add a new level of high performance thermal imaging with 640 × 480 resolution for greater image detail and accuracy, a 4.3 touchscreen, Wi-Fi mobile device connectivity, and more.