Technical Guidance
What is the difference between the PathFindIR II and Boson, Quark2, Tau2 cores?
Read the StoryTechnical Guidance
What is the influence of the camera temperature on the pixel readings? Can this be corrected by a linear model?
Read the StoryTechnical Guidance
How are FLIR's microbolometer arrays packaged? Are they under vacuum? Why?
Read the StoryTechnical Guidance
Does the PathFindIR II come with the same accessories as Tau2 and Quark2 cameras?
Read the StoryTechnical Guidance
How does FLIR test its thermal camera cores and lenses for sealing to IP67? Is a vacuum test used?
Read the StoryTechnical Guidance
Does operating Tau2, or Quark2, or legacy Photon cameras at less than 9 Hz reduce the camera power consumption?
Read the Story