FLIR ONE® Device Compatibility
Before introducing the new wireless and multiplatform camera FLIR ONE Edge Pro, FLIR offered two different versions for each of the FLIR ONE Pro, Pro LT and Gen 3 models: an Android version with a USB type-C connector and an iOS with a Lightning connector.
The new FLIR ONE Edge Pro does not require a physical connection to the camera, allowing it to work seamlessly with either an Android or iOS system.
Android Device Compatibility
To be compatible with FLIR ONE Pro, FLIR ONE Pro LT and FLIR ONE Gen 3, the mobile device must have a USB-C or micro USB charging port.
FLIR ONE App version | Compatible Android version | Supported Camera Models | Phone Requirements |
---|---|---|---|
v4.0.0 |
Android 13
Android 12
Android 11
|
FLIR ONE Edge Pro
FLIR ONE Pro
FLIR ONE Pro LT
FLIR ONE Gen 3
|
|
v3.6.1 |
Android 10
Android 9
|
FLIR ONE Pro
FLIR ONE Pro LT
FLIR ONE Gen 3
|
|
Will it work with my phone case? |
The innovative FLIR ONE Edge Pro wirelessly connects to your smart device so you can easily inspect targets that are out of reach – or clip it onto your phone or tablet for one-handed operation. With the OneFit™ feature, the FLIR ONE connector will adjust up to an additional 4 mm in length. This length is compatible with most protective cases, so you don’t have to choose between thermal vision and safeguarding your device. We have not tested all cases, but have picked many of our favorites. The 4-mm extension will not complete a connection through the Lifeproof and Otter Box Defender cases, so an OTG compliant adapter will be required (not offered by FLIR). |
Note: Sometimes 64-bit chipsets are limited to work as 32-bit version (armeabi-v7a). To confirm if your phone is compatible with the FLIR ONE App necessary to operate the camera you can install the app third party AIDA64 and confirm your phone Supported ABIs.
Android Owners with micro-USB port
Have an Android device with micro-USB port but want to use a FLIR One with a USB-C connector? Please be sure to buy a Type C OTG Adapter, USB-C Female to Micro-USB Male OTG (On the Go), to your cart before purchasing. It can also be purchased from Amazon.com.
iOS Device Compatibility
To be compatible with FLIR ONE Pro, FLIR ONE Pro LT and FLIR ONE Gen 3, the mobile device must have a Lightning charging port.
Model | Comments |
---|---|
iPhone 14 series |
Supported use with iPhones and iPads that have iOS 14 or newer OS versions. The accessory has been designed to connect specifically to these models and has been certified by the developer to meet Apple performance standards. Apple is not responsible for the operation of this device or its compliance with safety and regulatory standards. Please note that the use of this accessory with iPod, iPhone, or iPad may affect wireless performance. |
iPhone 13 series | |
iPhone 12 series | |
iPhone 11 series | |
iPhone X series | |
iPhone 8 series | |
iPhone 7 series | |
iPhone SE Gen 2 | |
All iPads with Lightning connector and the iOS required.
|
|
Will it work with my phone case? |
With the OneFit™ feature, the FLIR ONE connector will adjust up to an additional 4 mm in length. This length is compatible with most protective cases, so you don’t have to choose between thermal vision and safeguarding your device. We have not tested all cases, but have picked many of our favorites. The 4-mm extension will not complete a connection through the Lifeproof and Otter Box Defender cases, a lightning extender will be required (not offered by FLIR).Important note for FLIR ONE Gen 1 owners |
We regret to inform the FLIR ONE Gen 1 is not compatible with the latest App v4.2.0 for iOS 13 and above released only for iPhone 6S and above. However, the FLIR ONE Gen 1 keeps functioning on the iPhone 5/5S with iOS 12.5.3