Flir MIX Webinar: One Dataset with Spatial and Temporal Alignment


Until now, researchers have had to choose between thermal and visible imaging: One reveals heat signatures while the other provides structural detail. Recording both and trying to align them manually — or harder still, synchronizing them temporally — can be inconsistent and time consuming. The result is data that's close but never quite complete.
This 60-minute webinar will explore a recent technological innovation in imaging that provides a solution to this long-standing challenge — visible and high-performance infrared cameras that work together with specialized software to deliver one dataset with perfect spatial and temporal alignment. The program will provide insight into the previous challenges of simultaneous thermal and visible imaging and discuss the new thermal imaging solution that captures and synchronizes high-speed thermal and visible imagery at up to 1,000 frames per second.