FLIR Announces Multiple Cameras for Critical Infrastructure and Safe City Security

Three New Pan-Tilt-Zoom Security Cameras Provide Long- or Short-Range Perimeter Protection in All Conditions

ARLINGTON, Va., December 19, 2019 – FLIR Systems, Inc. (NASDAQ: FLIR) announced three dome-shaped, Pan-Tilt-Zoom (PTZ) security cameras, including two dual-sensor camera series for critical infrastructure locations, the FLIR Elara DX-Series and the FLIR Saros DM-Series, and a high-resolution visible camera for safe city deployments, the FLIR Quasar 4K IR PTZ. The latest FLIR security products offer multiple lens options for long- and short-range needs to enable accurate perimeter protection of critical infrastructure, remote facilities, and in urban city environments, day or night. 

1200x628_DM-O_Straight.jpg

Critical infrastructure sites, such as utility substations and transportation centers, have significant and often increased security requirements. The latest FLIR Systems cameras featuring thermal imaging and 4K high-resolution sensors, the Elara DX-Series and Saros DM-Series, help deliver superior perimeter security protection where it matters most. With the ability to see through fog, rain, sun glare, and snow, both series provide the ability to spot heat signatures at all hours. The FLIR Elara DX-Series features longer viewing range capabilities, infrared illumination, and a wiper blade that can be remotely operated for use in harsh conditions to ensure a clear view. The more compact Saros DM-Series provides shorter viewing range capabilities in a weatherized housing. Both series offer eight lens options, enabling customers to choose the most appropriate lens for their application. 

For the growing metropolitan city safety and security market, the Quasar 4K IR PTZ delivers high-resolution visible video quality with the best-in-class low light capabilities to give operators superior monitoring in large coverage areas. 

1200x628_Quasar_4K_IR_PTZ.jpg

Providing VMS integration with FLIR United VMS and all major platforms, these latest FLIR security cameras can provide a comprehensive end-to-end experience with a seamless integration to the FLIR United VMS platform or a complementary solution with integration available to all major platforms.

“With our latest products, FLIR is delivering advanced cameras purpose-built for perimeter protection and the evolving security needs of critical infrastructure sites and cities,” said Travis Merrill, President of the Commercial Business Unit at FLIR. “For surveillance in critical environments, including utility substations, airports, train stations, or stadiums, these perimeter protection cameras are designed to withstand harsh environments to help keep sites secure and people safe.”

The Saros DM-Series is available for purchase immediately while both the Elara DX and Quasar IR PTZ will be available in the first half of fiscal 2020, all through FLIR Systems’ network of established dealers and integrators.

To learn more about these new FLIR security camera solutions, please visit FLIR.com/Security. 

                                           -###-

About FLIR Systems, Inc.

Founded in 1978, FLIR Systems is a world-leading industrial technology company focused on intelligent sensing solutions for defense, industrial, and commercial applications. FLIR Systems’ vision is to be “The World’s Sixth Sense, creating technologies to help professionals make more informed decisions that save lives and livelihoods. For more information, please visit www.flir.com and follow @flir.

相关文章

奖项

FLIR Receives Two Security Awards at ISC West 2019

Read more
奖项

FLIR Saros Security Camera Wins Detektor International 2018 Award

Read more
产品新闻

Introducing FLIR Saros Dome Outdoor Perimeter Security Cameras

Read more
Back to top