Safe, Low-Cost Diagnosis of Concrete Structures with High-Definition Thermal Imaging

Concrete structures—usually typified by expresswaysare the foundation of the infrastructure systems that make our lives richer and more convenient in modern communities. The construction of concrete structures has been further promoted under high economic growth. However, as these structures age and decay with the passage of time, they begin to impede safety when broken pieces of concrete and other building materials fall off and scatter.

With the aging of social infrastructure systems becoming an urgent issue, the Japanese company West Nippon Expressway Engineering Shikoku Company Limited has developed a technology called “IrBAS” using FLIR A6701sc thermal imaging cameras. Currently, the team—including Mr. Matsuda, Mr. Hashimoto, and Mr. Hayashi—is using the IrBAS as an aging countermeasure for maintaining concrete structures.

Drawbacks of Conventional Concrete Testing

Previously, hammering tests for the entire surface of expressway bridges and other concrete structures were performed as a maintenance countermeasure. In such work, the inspector uses a hammer to check for problems on site, particularly signs that concrete pieces are in danger of peeling away and falling off due to the corrosion of steel bars. But this method of testing has drawbacks, including safety issues due to the high-place work settings, the time required to set up and move the scaffolding, and the declining number of inspectors.

j-system-jr-image2.jpg

Infrared thermography is used as a method for detecting defects within concrete structures remotely, without directly accessing the building. With this method, a difference in internal structure owing to defects is expressed as a temperature difference in the concrete surface, and the temperature difference is photographed.

“The IrBAS is capable of photographing and diagnosing a wide area at one time by thermography, which helps dramatically reduce inspection time and effort,” says Mr. Hashimoto. When testing, it's extremely time-consuming to hammer all inspection points one by one on the concrete surface, which covers several thousands to several tens of thousands of square meters.

But with the IrBAS, healthy parts and abnormal parts of the structure are roughly selected before hammering, and only the parts diagnosed as abnormal are subjected to a hammering test. This procedure dramatically reduces the number of inspection points. In addition, the photographed data can be retained for later aging examinations.

Decision Thermal Image Analysis Image

Observation

image1.png image2.png

Attention

image6.png image3.png

Caution

image4.png image5.png

Choosing the Best Technology for the Job

With the IrBAS, even if the object is far away, the inspector can shoot while standing on the ground by using a telephoto lens. This mechanism reduces the amount of high place work required and greatly improves the safety of inspectors. “The IrBAS classifies abnormal parts into three stages—caution, attention, and observation, which are identified using three different colors," says Mr. Hashimoto. "The image data are analyzed for temperature differences, shapes, areas, and other factors by a unique algorithm, to identify problems.”

In pursuit of an optimal inspection method, the team examined the impact on diagnostic results of differences between uncooled and cooled thermal imaging cameras, differences in wavelength used for measurement, and differences in parameters among various types of hardware, such as detectors and lenses. Such examinations turned out to be a study of thermography itself.

Starting with empirical research on the uncooling type, the team then studied the cooling-type QWIP and finally arrived at the indium antimonide type, which is sensitive to intermediate wavelengths.

The cooling type is more sensitive than the non-cooling type. Some units of the same cooling type are affected more than the others in a long wavelength band, by reflections from the sky or the opposing surface. These reflections affect the diagnostic results as a disturbance of acquired image data.

“We finally selected the indium antimonide-type thermography from FLIR Systems,” says Mr. Hashimoto. The FLIR A6701sc camera currently in use is an indium antimonide type, having a temperature resolution of 0.02°C and a wavelength of 3–5 μm.

Comparison of impacts of sky reflection:

Visible image

J1.jpg

Thermal image Insb (1.5–5.1μm)

Temperature difference (A-B) 0.2°C

J2.jpg

Thermal image QWIP (8–9μm)

Temperature difference (A-B) 1.0°C

J3.jpg

Thermal image μ porometer (8–14μm)

Temperature difference (A-B) 2.0°C

J4.jpg

To detect defects of within a concrete structure, a temperature difference is photographed on the concrete surface. The surface of a concrete structure is highly prone to temperature variances owing to differences in thickness of components and color unevenness, in addition to the generation of free lime owing to rainwater infiltration and the adhesion of foreign matter and irregularities caused during the construction phase. It's not easy to distinguish between temperature differences caused by these factors and temperature differences caused by internal defects.

But after many years of research, the team found that all parts judged to be healthy in diagnostic results with the IrBAS are confirmed as having no abnormality in subsequent hammering tests. As a result, the number of inspection points required has been reduced to a large extent. Furthermore, the IrBAS makes it possible to distinguish among different types of damage, such as floating, peeling, water leakage, and contamination by foreign substances.

Example (Floating):

Visible image

image12.png

Thermal image

image10.png

Analysis image

image11.png

Example (Contamination by foreign substances):

Visible image

image9.jpeg

Thermal image

image7.png

Analysis image

image8.png

“Through deep learning, we are seeking to increase the accuracy of the system not only to be able to make distinctions between sound and abnormal parts, but also to grasp the details of each abnormality, by further expanding the inspection results as teaching data," says Mr. Hashimoto. "Furthermore, we will introduce an analysis server, build an automatic judgment system, and utilize AI.”

Concrete structure diagnosis of bridges can be applied to general roads, railways, and buildings, as well as to expressways. Learn more about FLIR solutions for infrastructure safety and maintenance: www.flir.com/security/total-solutions-for-critical-infrastructure

Articles connexes

Étude de cas

La caméra thermique FLIR permet aux scientifiques de capturer et d'enregistrer les répartitions et les variations des événements thermiques dans le couvert végétal

Read more
Étude de cas

Preventing Disaster at Steel Mills with Continuous Thermal Imaging

Read more
Étude de cas

FLIR Thermal Imaging Enables Autonomous Inspections of Mining and Trucking Vehicles in Australia

Read more
Back to top