Teledyne FLIR Strengthens Perimeter Security Portfolio with First Commercial Ground-Based Radar and New Multispectral Camera Series

Elara R-Series Radars and FH-Series Cameras Improve Intruder Tracking, Geolocation and Alerts for Faster Threat Detection

THOUSAND OAKS, C.A., September 23, 2021 – Teledyne FLIR, part of Teledyne Technologies Incorporated (NYSE:TDY), announced today the release of new additions to its perimeter security portfolio for critical infrastructure; Elara R-Series Commercial Ground Security Radars and the FH-Series Multispectral Fixed Cameras. A first for Teledyne FLIR, the Elara R-Series is the ideal commercial radar system for industrial commercial applications, increasing detection coverage, auto-tracking, dynamic mapping and position intelligence of intruders. Part of the Teledyne FLIR premium family of multispectral security cameras, the FH-Series delivers both intrusion detection and video verification through its high-resolution thermal and visible imaging capabilities. These features plus the ability to capture vital details using 4K imagery enables security personnel to properly identify and assess situations, significantly improving response time.

The Elara R-Series introduces compact ground radars built to work within larger security systems to provide advanced warning of both human and vehicle intrusions beyond the fence line, while continuously tracking and precisely locating multiple targets. This series consists of two models, each designed with regional certifications in mind: the Elara R-290, which is compliant with United States Federal Communications Commission (FCC) guidelines, and the Elara R-190, which is Conformité Européenne (CE)-compliant for Europe. The Elara R-290 features a 90-degree field of view, up to a 400-meter range for vehicle tracking, a 200-meter range for human tracking, and provides wide-area protection as well as situational awareness beyond the fence line; the Elara R-190 offers a 300-meter range for vehicles and 125 meters for humans. These products are designed for reliable detection in all weather and lighting conditions. The radars’ auto-tracking feature helps to direct pan-tilt-zoom surveillance sensors in the right direction; the radars also help expand coverage area and significantly minimize false alarms. In addition, both models can provide security personnel with precise, real-time data, 24/7.

The FH-Series are ruggedized, multispectral fixed cameras that integrate industry-leading thermal imaging for detection with 4K visible imaging to help identify intruders in harsh perimeter security settings. Critical infrastructure facilities will benefit from technological advancements, such as highly-accurate convolutional neural network (CNN)-based video analytics for both thermal and visible spectrums, which minimize false alarms and aid in geo-locating threats for superior situational awareness. The on-board scheduling tool gives the operator the ability to select the type of analytics used to make detections based on time of day, business hours, and seasonality. Additionally, radiometric versions of the FH-Series can be used for early fire detection applications to help critical sites operate safely and efficiently.

“Teledyne FLIR is committed to equipping security directors with technologies that empower them to protect their facilities and personnel at mission critical sites,” said Kai Moncino, Global Business Development Manager, Security at Teledyne FLIR. “The Elara R-Series and FH-Series are built to enhance perimeter protection, providing accurate detection and alerting of threats. As with all of our new products, the Elara R-Series and FH-Series are designed with the latest cyber-hardening features for added security and peace of mind.”

To learn more about the FH-Series ID, please visit www.flir.com/FH-Series-ID.

To learn more about the FH-Series R, please visit www.flir.com/FH-Series-R.

To learn more about the Elara R-190 please, visit www.flir.com/R-190.

To learn more about the Elara R-290 please, visit www.flir.com/R-290.

 

-###-

 

About Teledyne FLIR

Teledyne FLIR, a Teledyne Technologies company, is a world leader in intelligent sensing solutions for defense and industrial applications with approximately 4,000 employees worldwide. Founded in 1978, the company creates advanced technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.teledyneflir.com or follow @flir.

About Teledyne Technologies

Teledyne Technologies is a leading provider of sophisticated digital imaging products and software, instrumentation, aerospace and defense electronics, and engineered systems. Teledyne's operations are primarily located in the United States, the United Kingdom, Canada, and Western and Northern Europe. For more information, visit Teledyne's website at www.teledyne.com.

Articles connexes

Récompenses

FLIR Wins 2021 Govies Government Security Awards for Perimeter Protection

Read more
Actualités sur les produits

FLIR Systems étend son offre de caméras de sécurité Quasar à lumière visible avec les modèles haut de gamme Premium Mini-Dome et Bullet Series

Read more
Actualités sur les produits

FLIR Adds New Advanced Features to United VMS with 9.0.1 Update

Read more
Back to top