Which Lenses can be used with the Thermal Fusion feature?

Thermal Fusion function only works with built-in or standard IR lens 24° / 25°.

Cameras that feature Thermal Fusion:

FLIR T-Series (T360, T400) uses 25° IR Lens
FLIR B-Series (B360, B400) uses 25° IR Lens

FLIR 600 Series (B620, B660, P620, P640, P660, SC620, SC660) uses 24° IR Lens 

Back to top