Stopping Small Heat Problems Before They Become Big Outages

The Earliest Fire Detection Technology on the Market

In the data center, smoke detection is essential, but smoke is not the first sign of failure. Heat is. While air-sampling systems wait for combustion by-products to travel through fast-moving airflow, thermal imaging continuously monitors large areas for abnormal temperature rise at the source. This gives operators the advantage of earlier insight, more accurate localization, and a stronger predictive maintenance strategy, reducing the chance of fire occurring at all, while also enabling faster, more precise response when tied into the fire alarm system.

A graph showing the timeline of fire development against the extent of damage, illustrating the stages at which different detection technologies intervene. 

This graphic shows a simple truth: the earlier a developing fire is detected, the more options a facility has to prevent damage, avoid downtime, and protect critical infrastructure. In data centers, that matters enormously. 

NFPA 75 exists specifically to protect information technology equipment and equipment areas from fire damage, while Uptime Institute’s 2024 analysis found that outages remain expensive: 54% of surveyed operators said their most recent significant outage cost more than $100,000, and 16% said it cost more than $1 million. Uptime also found that power issues remain the most common root cause of serious and severe data center outages.

Fire does not begin with flames. It begins with heat. Long before smoke particles form, long before a flame detector triggers, and long before a sprinkler system activates, a developing thermal event is already generating an infrared signature that is detectable by infrared imaging.

Thermal cameras move detection to the very earliest point on that timeline: the heating phase, before any other technology has registered anything at all. Most current fire detection systems are designed to contain a fire once it starts, which is often too late. Using non-contact thermal monitoring, automated infrared cameras can pinpoint hot spots and provide live temperature data updates up to 60 times per second.

In a data center environment, where overheating servers, stressed UPS systems, and high-density electrical infrastructure represent everyday fire risk, that lead time is not a marginal advantage. It is the difference between a maintenance callout and a major incident.

Built to Watch Without Stopping

For thermal fire detection to fulfil its potential, the hardware doing the watching must be as reliable as the facility it protects. A fixed thermal camera monitoring a UPS array or primary switchgear room is only as valuable as its availability. Flir cameras operate across a temperature range of -40°C to 85°C without calibration drift, with a mean time between failures of 87,000 hours—nearly double the 45,000 to 60,000 hours offered by competing systems. For a fixed monitoring deployment with a 10-to-15-year equipment lifecycle, that reliability is not a specification footnote. It is the foundation of a fire detection program that can be depended upon continuously, not merely periodically.

A camera that is present, accurate, and operational at 3 am on a Sunday morning—when the fault that would have been caught at the Tuesday inspection is already developing—is the difference between a facility that detects early and one that only believes it does.

Flir sees the thermal instability developing in the battery system directly, at the heating stage, and alerts the operations team while the intervention is still straightforward.

A New Certification Changes the Baseline

NFPA 75, updated in 2024, governs fire protection requirements for IT equipment areas and treats fire and thermal events as existential risks in critical environments. UL-certified thermal cameras are designed to satisfy those requirements—not as a supplement to existing smoke detection, but as a certified replacement for it. For fire engineers, architects, and performance-based design consultants specifying new data center builds or major refurbishments, this certification opens a conversation that was not previously available: the ability to specify the earliest detection technology on the market as the primary fire detection system, within a fully code-compliant framework.

 

Request Info

Optin

By submitting you agree to FLIR's privacy policy and cookie policy.

Back to top