Application Spotlight: Inspection for Methane Leaks in a Combined Cycle Power Plant

Quickly and Safely Inspect for Methane Leaks and Heating Issues Related to Electrical/Mechanical Applications

Natural gas fired power plants are becoming more prominent simply because they are less expensive to build, are very efficient, and produce less pollution than plants run by coal, as an example. When using methane gas, it is very important to have a regular predictive maintenance plan that includes an inspection of critical components and other hardware.

Traditional methane leak detection methods are costly, time consuming and are not a reliable way of finding the source of a given leak. Learn how FLIR's solution can help improve safety, improve efficiency, and help reduce the impact on the environment.

Download the Application Spotlight

Back to top