With A320, IR Monitor, which is included, should be used for camera setup including changing range.
With A325, ThermaCAM Researcher or FLIR ResearchIR is in full control of all camera parameters.
See also the Command and resource documentation (T559002 and T559003) that are downloadable from the manual download page.