The best way to really experience the intuitive yet powerful ResearchIR 4 software that is included with FLIR’s R&D/Science Solutions is to try it first hand by downloading and running any one of the Self Viewing Files (SVF) below.
Not familiar with FLIR ResearchIR 4 Self Viewing Files? Self Viewing Files or SVF’s are one of the many great ways to share data that is unique to ResearchIR 4. What happens is our software takes a copy of ResearchIR and wraps it around the dataset, creating a single executable file. You can then distribute that file without any licensing requirements, and the recipient can then open the file and have nearly all the same functionality with that data set as if they owned a copy of ResearchIR 4 and had it installed on their machine. Below is a collection of SVF’s we’ve created for multiple applications using various FLIR R&D/Science thermal cameras.
To get started, simply download one of the SVF’s below and run it on any Windows XP, Windows 7, Windows 8, or Windows 10 computer. We can’t wait for you to get hands on with the new ResearchIR 4 today!
High Definition Airbag Deployment Testing
High Definition and high speed thermal measurement and testing on airbag deployment.
Airbag Deployment Testing
High speed thermal measurement and testing on side airbag deployment.

Airplane Tracking and Target Signature
Airplane tracking and target signature with thermal camera.
Car Exhaust CO2 emissions
CO2 “warm” MWIR filter used to image otherwise invisible gas.
Cow CO2 Exhalation
Using a CO2 filter and FLIR High Sensitivity Mode Filter even animal exhalation is visible.
High Speed Droplet
FLIR high speed, high resolution thermal cameras are used to study droplet temperature changes.
High Definition Imagery of Dolphins Jumping
High Definition thermal imagery of dolphins jumping.
Bio Medical Testing on Lamb Heart
Thermal imagery and measurement of injection into a lamb heart.
Thermal Failure Analysis on Optical Transceiver
Failure analysis on optical transceiver using thermal camera.
High Definition Temperature Measurement on Electronics Board
High Definition thermal measurement and testing on Printed Circuit Board (PCB).
Electron Beam Welding
FLIR high speed MWIR cameras sees into vacuum chamber to look at electron beam weld profile.