Status of driver "This device cannot start", after connecting the BCAM camera to the USB port of a computer (desktop or laptop). Driver Date: 7/1/2001 Driver Version: 5.1.2600.0
Here are some suggestions that may solve the problem:
- Go into the camera setup menu and make sure "USB Cable" is set to "Standard" mode.
- If you are using a BCAM SD make sure the SD card is installed in the camera slot, which is to the right of the USB connector.
- Go into the camera setup menu and select "Restore default". This will reset the camera to original factory settings.
- Try a different USB cable.
In one case, solution was the SD card had to be installed in the camera slot in order to enable a mass storage drive.